Hello There,
I am working on custom IMX7D board based on imx7 dual sabre board. I am trying to use the same uboot code from reference design, but unlike the reference board, in my design I have only single DDR3 of 4Gb. So are there any changes which I should make in the uboot or will it take care itself?
Thanks in advance.
Hello,
Use Chapter 3 (Porting U-Boot) of i.MX_Porting_Guide.pdf in Linux documentation.
https://www.nxp.com/webapp/Download?colCode=imx-yocto-L4.14.98_2.0.0_ga
The following tools may be helpful:
i.MX6/7 DDR Stress Test Tool V3.00
https://community.nxp.com/docs/DOC-152468
Have a great day,
Yuri.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.