Hello all,
Currently am working with nitrogen6x board.
Earlier the device was booting, by mistakenly i did something in u-boot environment, now it is not booting.
showing the below information and after that it is stopping.
U-Boot 2014.07-00136-gf870252 (Sep 22 2014 - 09:16:34)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: WDOG
Board: Nitrogen6X
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB
auto-detected panel wvga-rgb
Display: wvga-rgb (800x480)
In: serial
Out: serial
Err: serial
Net: using phy at 6
FEC [PRIME], usb_ether
U-Boot >
Please help on this it is very urgent.
Hi Madhu,
It looks like you've either erased the bootcmd varialble or set bootdelay to -1 which disables autoboot.
My advice, clear your saved environment:
> env default -a
> saveenv
> reset
Regards,
Gary