Ubuntu 14.04.4 on i.MX6 SoloX Sabre SD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ubuntu 14.04.4 on i.MX6 SoloX Sabre SD

1,685 Views
xenodigm
Contributor I

Dear All.

I'm trying to install Ubuntu 14.04.4 core on i.MX6SX Sabre board.

Attached File is the shell script for installing toolchain-4.9-2014.09, u-boot-v2015.04_3.14.52_1.1.0, linuxkernel-3.14.52_1.1.0 and ubuntu-core-14.04.4.

 

Procedure of attached shell script)

1. Downloading toolchain-4.9-2014.09.

2. Downloading and  building u-boot-v2015.04_3.14.52_1.1.0 source.

3. Downloading and  building linuxkernel-3.14.52_1.1.0 source.

4. Preparing SD.

5. Installing u-boot and kernel image files on SD.

6. Downloading and install ubuntu-core-14.04.4.

 

As follows, it stopped at "Stopping System V runlevel compatibility [ OK ]".

I attach the shell script and log file.

Can you help-me?

 

 

--------------------------------------------------------------------------------

U-Boot 2015.04 (Feb 23 2016 - 23:51:46)

 

CPU:   Freescale i.MX6SX rev1.2 at 792 MHz

CPU:   Temperature 35 C

Reset cause: POR

Board: MX6SX SABRE SDB

 

........................................................................................

........................................................................................

* Starting Mount network filesystems                                    [ OK ]

* Stopping Failsafe Boot Delay                                          [ OK ]

* Starting System V initialisation compatibility                        [ OK ]

* Starting configure virtual network devices                            [ OK ]

* Stopping Mount network filesystems                                    [ OK ]

* Stopping System V initialisation compatibility                        [ OK ]

* Starting System V runlevel compatibility                              [ OK ]

* Starting save kernel messages                                         [ OK ]

* Starting regular background program processing daemon                 [ OK ]

* Stopping save kernel messages                                         [ OK ]

* Stopping System V runlevel compatibility                              [ OK ]

------------------------------------------------------------------------------------------------------------

Original Attachment has been moved to: log.txt.zip

Original Attachment has been moved to: imx6sx_sabresd_3.14.52.sh

Labels (2)
0 Kudos
Reply
1 Reply

618 Views
joanxie
NXP TechSupport
NXP TechSupport

I haven't tested the same procedure as yours, but I found some helpful document to you for reference

Linux on the i.MX6 sabre sd platform in a few commands

How to create ubuntu hardfloat rootfs for imx6d/q

0 Kudos
Reply