UUU monitor USB paths

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UUU monitor USB paths

1,236件の閲覧回数
Raymond2
Contributor I

Hi, 

When UUU uses "-m" to monitor USB path, it will get stuck during fastboot because the path has changed. 
This is mentioned in the UUU pdf file as well:
"Notes: Some board supports super speed (USB3.0). USB 3.0 port path is difference USB 2.0. If use -m to filter port, you need add USB 3.0 port number otherwise fastboot will not be detected."

Currently I used "uuu -lsusb" to get the USB path of my device, but it does not give the USB 3.0 port number. Currently I'm using USB device tree viewer to get the number, but its not suitable if I want to write  a script to automate this process. Different PC might have different paths, so the script has to be able to determine itself which paths to choose for "uuu --match". 

May I know if you have any suggestion for this?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,191件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Raymond2 

Have you tried latest uuu?

If yes, please create an issue here : https://github.com/nxp-imx/mfgtools/issues

Best Regards

Zhiming

0 件の賞賛
返信

1,175件の閲覧回数
Raymond2
Contributor I
Hi Zhiming,
I think this is not as issue but trying to understand if there's a better way to get USB 3.0 path.
0 件の賞賛
返信