Hi,
I used VS2019 compile uuu-1.3.191 on Win10. However, I got error as below:
Could some one sent me the file 'gitversion.h'? Thanks.
We could not see your error information.
UUU is an evolution of MFGTools. The attachment is an introduction of UUU. Please download uuu.exe and follow the UUU introduction.
Here are some running examples. If you are not familiar with uuu, you can refer to them firstly.
Under Windows (should be as admin):
Under Linux:
If you download BSP release from nxp.com, you could find a file uuu.auto in the package. This is a preset script that can be executed directly (default for EMMC). You could change the script based on your requirement. Copy the uuu.exe under the release package, then execute the instructions.
Sorry to find that the picture was not showed. The errors are:
Error (active) E1696 cannot open source file "gitversion.h" libuuu D:\Test\DBSMX8X\UUU_1.3.191\uuu-1.3.191\libuuu\version.cpp 32
Error C1083 Cannot open include file: 'gitversion.h': No such file or directory libuuu D:\Test\DBSMX8X\UUU_1.3.191\uuu-1.3.191\libuuu\version.cpp 32