USB to ehternet adapters for linux:imx6sx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB to ehternet adapters for linux:imx6sx

1,723 Views
czur
Contributor III

Hi,

I am trying to connect a USB to ethernet adapter(ASIX AX88XXX) to the USB OTG1 port on the imx6sx custom board.

I have setup the device tree for the usbotg1 as below, I have enabled the USB net driver CONFIG_USB_NET_AX8817X along with USB_USBNET. but when I plug in the device, the relevant driver is not probed instead the usb device is just populated as Bus 001 Device 001: ID 1d6b:0002 as below: am I missing any other driver or config that is preventing the driver from getting probed?

Listing when the device is plugged in:

# ci_hdrc ci_hdrc.0: EHCI Host Controller
ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 2
ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb2: Product: EHCI Host Controller
usb usb2: Manufacturer: Linux 4.9.11-rt9 ehci_hcd
usb usb2: SerialNumber: ci_hdrc.0
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected

#
# lsusb -t
Bus 001 Device 001: ID 1d6b:0002

Device tree:

reg_usb_otg1_vbus: regulator@5 {
compatible = "regulator-fixed";
reg = <5>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usb_otg1>;
regulator-name = "usb_otg1_vbus";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
gpio = <&gpio1 9 GPIO_ACTIVE_HIGH>;
enable-active-high;
};

&usbotg1 {
vbus-supply = <&reg_usb_otg1_vbus>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usb_otg1_id>;
disable-over-current;
srp-disable;
hnp-disable;
adp-disable;
dr_mode = "otg";
status = "okay";
};

pinctrl_usb_otg1: usbotg1grp {
fsl,pins = <
MX6SX_PAD_GPIO1_IO09__GPIO1_IO_9 0x10b0
>;
};

pinctrl_usb_otg1_id: usbotg1idgrp {
fsl,pins = <
MX6SX_PAD_ENET2_COL__ANATOP_OTG1_ID 0x17059
>;
};

Labels (2)
0 Kudos
1 Reply

1,382 Views
igorpadykov
NXP Employee
NXP Employee

Hi Arun

one can try latest nxp linux L4.14.78_1.0.0 and ax88xx drivers
linux-imx - i.MX Linux kernel 

https://www.asix.com.tw/download.php?sub=driverdetail&PItemID=84 

some debugging hints can be found on
embedded linux - Asix usb to network adapter doesn't work (kernel 2.6.32.17) - Stack Overflow 

FAQs:
https://www.asix.com.tw/products.php?op=pItemdetail&PItemID=86;71;101 

If ASIX USB to LAN drivers cannot work fine on your USB to LAN device, please
refer to How to identify authentic ASIX USB to LAN Products document to double check
if your USB to LAN device includes a Non-authentic ASIX USB to LAN solution inside or
not? If yes, please contact the manufacturer of your USB to LAN device to get proper drivers directly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos