USB Linksys USB300M USB 2.0 Ethernet Adapter in not working in IMX53 QSB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Linksys USB300M USB 2.0 Ethernet Adapter in not working in IMX53 QSB

4,544 Views
praveen_ismd
Contributor I

Hi

I was using Linksys USB300M USB 2.0 Ethernet Adapter on Panda board with ubuntu server edition 11.10 and it was working fine, but the same adapter is not working on IMX53 QSB with ubuntu 10.04, can any one tell me the solution, how to make it work ?

Labels (2)
0 Kudos
Reply
15 Replies

2,545 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Praveen,

     Could you tell me the following information ?

(1)Could you see log infomation about USB3000M on console ?

(2)On console,Can we find USB new device on USB HOST ?

(3) Did you add the driver for USB3000M to kernel source code and recompile image for MX53QSB ?

Regards,

Weidong

0 Kudos
Reply

2,545 Views
praveen_ismd
Contributor I

I had not compiled the kernel, as i am using the image came with the board, and on console I cannot find any device.

0 Kudos
Reply

2,545 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Praveen,

     Would you like to paste linux booting log here ? Let me see it !

Regards,

Weidong

0 Kudos
Reply

2,545 Views
praveen_ismd
Contributor I

Hi Weidong

I am attaching the boot log file, but I am not able to see any USB300M, is it possible that kernel is not supporting it, and if so then, what can be possible solution.

0 Kudos
Reply

2,545 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Praveen,

     What usb devices did you connect to USB HUB ?

usb 2-1.2: new high speed USB device using fsl-ehci and address 3

usb 2-1.3: new low speed USB device using fsl-ehci and address 4

   Regards,

Weidong

0 Kudos
Reply

2,545 Views
praveen_ismd
Contributor I

One device is USB mouse and another is USB To ethernet convertor ie Linksys USB300M

0 Kudos
Reply

2,545 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Praveen,

    USB controller can emulate it and find new device, but system can't find it's drivers. So you will have to add USB300M for linux driver to i.mx53 platform, or compile it with arm-gcc compiler and load it into system by insmod command.

Regards,

Weidong

0 Kudos
Reply

2,545 Views
praveen_ismd
Contributor I

Hi Weidong,

Thanks for suggesting me up till now,

I downloaded the code for driver but i am not a able to compile it on board,

this is the link from where I downloaded the driver code http://www.asix.com.tw/download.php?sub=driverdetail&PItemID=86

Do i have to make modification in make file ?

This is the make file

CURRENT= $(shell uname -r)
TARGET= asix
OBJS= asix.o
MDIR= drivers/net/usb
KDIR= /lib/modules/$(CURRENT)/build

SUBLEVEL= $(shell uname -r | cut -d '.' -f 3 | cut -d '.' -f 1 | cut -d '-' -f 1 | cut -d '_' -f 1)

ifneq (,$(filter $(SUBLEVEL),14 15 16 17 18 19 20 21))

MDIR = drivers/usb/net

endif

EXTRA_CFLAGS = -DEXPORT_SYMTAB

PWD = $(shell pwd)

DEST = /lib/modules/$(CURRENT)/kernel/$(MDIR)

obj-m      := $(TARGET).o

default:

make -C $(KDIR) SUBDIRS=$(PWD) modules

$(TARGET).o: $(OBJS)

$(LD) $(LD_RFLAG) -r -o $@ $(OBJS)

install:

su -c "cp -v $(TARGET).ko $(DEST) && /sbin/depmod -a"

clean:

$(MAKE) -C $(KDIR) SUBDIRS=$(PWD) clean

.PHONY: modules clean

-include $(KDIR)/Rules.make

0 Kudos
Reply

2,545 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Praveen,

      I compiled a .ko file for your usb net module. you can try to load it on your board.

Regards,

Weidong

2,545 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Ok, Praveen and Grant,

     Let me paste content on how to adjust Makefile for Cross-compile based on ARM Platform here , Because original Makefile is for x86 .

/* The following is for Cross Compile*/

ARCH :=arm
KDIR := /home/weidong/myandroid/kernel_imx
CROSS_COMPILE :=/opt/freescale/usr/local/gcc-4.4.4-glibc-2.11.1-multilib-1.0/arm-fsl-linux-gnueabi/bin/arm-none-linux-gnueabi-

CC := $(CROSS_COMPILE)gcc
LD := $(CROSS_COMPILE)ld
NM := $(CROSS_COMPILE)nm
OBJCOPY := $(CROSS_COMPILE)objcopy

HOSTCC := gcc
export CC HOSTCC

PWD := $(shell pwd)

obj-m +=asix.o
default:
$(MAKE) -C $(KDIR) M=$(PWD) modules
clean:
rm -rf *.o *.ko

    Then run "make" command in current path where Makefile exists. We can get aisx.ko file. this is the driver for USB net card---USB300M

Regards,

Weidong

0 Kudos
Reply

2,545 Views
praveen_ismd
Contributor I

Thanks Weidong for your help I had solved the problem many weeks ago !!

0 Kudos
Reply

2,545 Views
praveen_ismd
Contributor I

Also according to make file after compilation I have to install it in /lib/modules/$(CURRENT)/kernel/drivers/net/usb

but there is no such folder in QSB


0 Kudos
Reply

2,545 Views
admin
Specialist II

Praveen, were you able to fix your compile problem and get the driver and adapter working?

0 Kudos
Reply

2,545 Views
praveen_ismd
Contributor I

Hi Grant,

I was able to solve the problem.

0 Kudos
Reply

2,545 Views
admin
Specialist II

Great.  I'm glad you were able to solve it.

Regards,

Grant

0 Kudos
Reply