Hi gxf
seems not according to linux ubifs documentation
linux/ubifs.txt at master · spotify/linux · GitHub
some workarounds are suggested on
Force fscheck ubifs - NETGEAR Communities
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
By default, about 2% of the whole chip size (20/1024 PEB) are reserved for bad blocks handling. If the number of blocks that turn bad exceeds that allocation, an error message will be printed and UBI will switch to read-only mode.
Can I improve the bad block handling size to reduce the possibility of errors?
If I can, what should I do?
this is general linux question and may be posted on kernel mail list
Majordomo Lists at VGER.KERNEL.ORG
Best regards
igor