UART GPS ANDROID 6.0.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART GPS ANDROID 6.0.1

3,098 Views
leonardoprates
Contributor III

I need enable a UART GPS in Android 6. My board is similar to SabreSD. I can see NMEA data in console using cat /dev/ttymxc3. But how I tell to Android use this UART4 to get and parse NMEA?

Labels (3)
0 Kudos
3 Replies

1,120 Views
leonardoprates
Contributor III

I have used this code GitHub - kconger/android-serial-gps-driver: Android Serial GPS Driver  and I get GPS working. I have another issue that I can't get AGPS working. I'm using this gps.conf. Could anyone give me directions? For supl.google.com is certificate necessary and how get one?

NTP_SERVER=br.pool.ntp.org

NTP_SERVER=0.br.pool.ntp.org

NTP_SERVER=1.br.pool.ntp.org

NTP_SERVER=2.br.pool.ntp.org

NTP_SERVER=3.br.pool.ntp.org

NTP_SERVER=south-america.pool.ntp.org

NTP_SERVER=0.south-america.pool.ntp.org

NTP_SERVER=1.south-america.pool.ntp.org

NTP_SERVER=2.south-america.pool.ntp.org

NTP_SERVER=3.south-america.pool.ntp.org

XTRA_SERVER_1=http://xtra1.gpsonextra.net/xtra.bin

XTRA_SERVER_2=http://xtra2.gpsonextra.net/xtra.bin

XTRA_SERVER_3=http://xtra3.gpsonextra.net/xtra.bin

# AGPS Daemon Call

DEFAULT_AGPS_ENABLE=TRUE

DEFAULT_USER_PLANE=TRUE

DEFAULT_SSL_ENABLE=FALSE

DEBUG_LEVEL=0

INTERMEDIATE_POS=1

ACCURACY_THRES=5000

#Active GOOGLE

### AGPS server settings GOOGLE ###

SUPL_HOST=supl.google.com

SUPL_PORT=7276

SUPL_SECURE_PORT=7278

SUPL_NO_SECURE_PORT=3425

############################

### AGPS alternative setting NOKIA ###

# SUPL_HOST=supl.nokia.com

# SUPL_PORT=7275

################################

### AGPS alternative setting  SONY ###

# SUPL_HOST=supl.sonyericsson.com

# SUPL_PORT=7275

################################

### AGPS alternative setting  T-MOBILE ###

# SUPL_HOST=10.176.29.225

# SUPL_PORT=7275

# SUPL_TLS_HOST=lbs.geo.t-mobile.com

##################################

#WiFi Position 1=”On”, 0=”Off”

ENABLE_WIPER=1

CURRENT_CARRIER=common

REPORT_POSITION_USE_SUPL_REFLOC=1

0 Kudos

1,120 Views
SergioSolis
NXP Employee
NXP Employee

Hello Leonardo,

The GPS conf looks ok.  Are you enabling the use of wireless networks and gps satellites?, do you have the logcat or how are you defininf that the a-gps is not working?

0 Kudos

1,120 Views
leonardoprates
Contributor III

The GPS fix takes too long and I can see in logcat this information:

07-07 20:48:29.873  1073  1086 D GpsLocationProvider: Reset GPS properties, previous size = 0

07-07 20:48:29.874  1073  1086 D GpsLocationProvider: GpsParamsResource: SUPL_HOST=supl.google.com

07-07 20:48:29.874  1073  1086 D GpsLocationProvider: GpsParamsResource: SUPL_PORT=7275

07-07 20:48:29.874  1073  1086 D GpsLocationProvider: GpsParamsResource: NTP_SERVER=north-america.pool.ntp.org

07-07 20:48:29.875  1073  1086 D GpsLocationProvider: GpsParamsResource: SUPL_VER=0x20000

07-07 20:48:29.875  1073  1086 D GpsLocationProvider: GpsParamsResource: SUPL_MODE=1

07-07 20:48:29.888  1073  1086 D GpsLocationProvider: GPS properties reloaded, size = 19

07-07 20:48:29.888  1073  1086 E GpsLocationProvider: no AGPS interface in set_agps_server

one.

07-07 20:48:29.924  1073  1073 W LocationManagerService: no network location provider found

0 Kudos