UART Debug port number in IMX7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART Debug port number in IMX7

877 Views
logeshs
Contributor II

Hi,

Kindly help me, which UART port is used for debugging in IMX7 (Part number # MCIMX7D7DVK10SC)

Thanks & Regards,

Logesh

Labels (1)
0 Kudos
2 Replies

668 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

 On iMX7DSABRESD board J11 connector is used for Debug UART (via USB).

According to board schematic: Debug UART1 is intended for Cortex-A7;

Debug UART2 for Cortex-M4.

   NXP BSP(s) uses such approach, but customers can use any available UART ports

(and pins) for their applications, assuming BSP modification, if needed. 

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

668 Views
logeshs
Contributor II

Also Kindly suggest shall we use any of below UART ports for debugging,

1. UART1 (Pin# D16 & D7)

2. UART2 (Pin# G28 & D20)

If we are not able to use the above ports for debugging kindly request you to provide correct the UART port ID with pin numbers.

Thanks & Regards

Logesh

0 Kudos