Hi guys,
I'm working on i.MX6UL custom board. Trying to configure SPI Flash (Model = Winbond W25Q128JV),
Here's the changes that I've made and the parts that I've added;
## arch/arm/dts/imx6ul-14x14-evk.dts;
+spi4 {
+ compatible = "spi-gpio";
+ pinctrl-names = "default";
+ pinctrl-0 = <&pinctrl_spi4>;
+ pinctrl-assert-gpios = <&gpio1 10 GPIO_ACTIVE_LOW>;
+ num-chipselects = <1>;
+ #address-cells = <1>;
+ #size-cells = <0>;
+ status = "okay";
+ flash: m25p80@0 {
+ #address-cells = <1>;
+ #size-cells = <1>;
+ compatible = "spansion,m25p80";
+ reg = <0>;
+ spi-max-frequency = <133000000>;
+ };
## board/freescale/imx6ul_14x14_evk.c;
+#define SPI_PAD_CTRL (PAD_CTL_HYS | \
+ PAD_CTL_SPEED_MED | \
+ PAD_CTL_DSE_40ohm | PAD_CTL_SRE_FAST)
-----------------------------------------------------------------------------------------------------------------------------
+#ifdef CONFIG_SPINOR
+/* pin conflicts with eim nor */
+static iomux_v3_cfg_t const ecspi1_pads[] = {
+ MX6_PAD_ENET2_TX_EN__ECSPI4_MOSI| MUX_PAD_CTRL(SPI_PAD_CTRL),
+ MX6_PAD_ENET2_TX_DATA1__ECSPI4_SCLK | MUX_PAD_CTRL(SPI_PAD_CTRL),
+ MX6_PAD_ENET2_TX_CLK__ECSPI4_MISO | MUX_PAD_CTRL(SPI_PAD_CTRL),
+ /* CS Pin */
+ MX6_PAD_JTAG_MOD__GPIO1_IO10 | MUX_PAD_CTRL(NO_PAD_CTRL),
+};
+static void setup_spinor(void)
+{
+ imx_iomux_v3_setup_multiple_pads(ecspi1_pads, ARRAY_SIZE(ecspi1_pads));
+ gpio_request(IMX_GPIO_NR(1, 10), "escpi cs");
+ gpio_direction_output(IMX_GPIO_NR(1, 0), 0);
+}
+int board_spi_cs_gpio(unsigned bus, unsigned cs)
+{
+ return (bus == 0 && cs == 0) ? (IMX_GPIO_NR(1, 10)) : -1;
+}
+#endif
-----------------------------------------------------------------------------------------------------------------------------
+#ifdef CONFIG_SPINOR
+ setup_spinor();
+#endif
-----------------------------------------------------------------------------------------------------------------------------
##configs/mx6ul_14x14_evk_defconfig
+CONFIG_DM_SPI=y
+CONFIG_DM_SPI_FLASH=y
+CONFIG_SPINOR=y
+CONFIG_WINBOND=y
+CONFIG_SPI_FLASH=y
+CONFIG_SPI_FLASH_BAR=y
+CONFIG_CMD_SPI=y
-----------------------------------------------------------------------------------------------------------------------------
##drivers/mtd/spi/spi_flash_ids.c
#ifdef CONFIG_SPI_FLASH_WINBOND /* WINBOND */
+ {"w25q128jv", INFO(0xef7018, 0x0, 64 * 1024, 256, RD_FULL | WR_QPP | SECT_4K) },
-----------------------------------------------------------------------------------------------------------------------------
##include/configs/mx6ul_14x14_evk.h
+#ifdef CONFIG_SPINOR
+#define CONFIG_CMD_SF
+#define CONFIG_SPI_FLASH
+#define CONFIG_SPI_FLASH_WINBOND
+#define CONFIG_SF_DEFAULT_BUS 4
+#define CONFIG_SF_DEFAULT_CS 0
+#define CONFIG_SF_DEFAULT_SPEED 133000000
+#define CONFIG_SF_DEFAULT_MODE SPI_MODE_0
+#endif
But I can't even open the SPI bus. Here's the terminal output when I try to 'sf probe'
=>sf probe
Invalid bus 0 (err=-19)
Failed to initialize SPI flash at 0:0 (error -19)
=>sf probe 4:0
Invalid bus 4 (err=-19)
Failed to initialize SPI flash at 4:0(error -19)
.
.
.
I dont know what I'm missing , I could use some help.
Thank you.
Hi berkay
one can recheck LUT, example can be found on
https://community.nxp.com/thread/446470
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I've checked the links but we're not sure that we need to use LUT and have to deal with registers . Also we're not using MFG so that answer will be so hard for us . Is there another way to probe an SPI flash?
Thanks for the answer.
Hi berkay
one can look at spi-nor n25q032 example:
flash: n25q032@0
uboot/board/freescale/mx6ul_14x14_ddr3_arm2/mx6ul_14x14_ddr3_arm2.c
mx6ul_14x14_ddr3_arm2.c\mx6ul_14x14_ddr3_arm2\freescale\board - uboot-imx - i.MX U-Boot
Best regards
igor
I did exactly the same configurations from the links but still getting the same errors , Invalid bus 4 (err = -19)
Also got the activated SPI conf scripts from the defconfig and configured the board header file from your link . Still missing something :/