Hello All
Hoping somebody can help me out here. This was suppose to have been something simple and easy. U-Boot has an example folder and a hello_world.c as a standalone application that gets compile as part of the U-Boot build and converted into a bin and srec file.
The U-Boot doc's said it should be as simple as issuing a "loads" and "go" command because the srec should have encoded the start and end address and entry point.
http://www.denx.de/wiki/DULG/UBootStandalone
So all I should have to do download it over serial read off the start address and type go with that address(-4)?..
Anyway it didn't work, quick look at the build and there is a text offset on the compiler line
-DTEXT_BASE=0xXXXXXXXX
and another offset on the linker line
arm-none-linux-gnueabi-ld -g -Ttext 0xYYYYYYYY.
Using these offsets actually allow the "loads" command to complete but it still fails to run with a go command.
Has anybody ran this demo and got it to work. Could you post a cut and past of the commands from the U-Boot prompt.
Thanks.
Hi, hope this is already resolved. But here is the clear explanation if it is not resolved.
Thanks Ed
So you have confirmed that Freescale not testing this demo when they port U-Boot to different platforms. (I'm on an ARD DDR3 board) I'll go back an try your suggestions shortly. (Freescale does a lot of good stuff, just wish they would have verified this on the boards before moving on to the Linux stuff.)
Rx.
Ed Sutter said:
Just to add to my own self-induced confusion, it appears that either 0x77800000 or 0x77c00000 works.
This confuses me because it appears that u-boot is loaded at 0x77800000, which would seem to indicate that loading hello_world at that same location would corrupt the running u-boot image, but it doesn't seem to cause any problem. I guess u-boot must relocate or something.
Just to add to my own self-induced confusion, it appears that either 0x77800000 or 0x77c00000 works.
This confuses me because it appears that u-boot is loaded at 0x77800000, which would seem to indicate that loading hello_world at that same location would corrupt the running u-boot image, but it doesn't seem to cause any problem. I guess u-boot must relocate or something.
Oops!!! Use 0x77c00000, not 0x77800000.
Ed Sutter said:
It appears to me that the load address of the hello-world app is not set correctly.
Looking at a dump of the hello_world ELF file shows me that the base address is 0x1c00000.
I then found that the makefile in that directory doesn't support the specifics of the imxQSB, so it defaults to that base address. I think all you need to do is modify examples/standalone/Makefile. The quick change is to set LOAD_ADDR to 0x77800000. I was then able to use tftpboot to launch hello_world successfully.
HTH
Ed
More information...
Sorry, should have included this the first time...
To do a TFTP boot (assuming you're on a linux machine), do the following...
1. LINUX: copy hello_world.bin to /tftpboot
2. UBOOT: using 'setenv', establish your IP environment (ipaddr, serverip, gatewayip & netmask)
3. UBOOT: tftpboot 0x77c00000 hello_world.bin
4. UBOOT: go 0x77c00000
To do an srecord transfer
1. UBOOT: loads
2. LINUX: use whatever means your serial port interface gives you to transfer hello_world.srec to the board.
3. UBOOT: go 0x77c00000
If you're running on a PC and need an alternative means of doing these downloads, you can use uCon as the terminal emulator and I can show you how to do that if needed.
HTH
It appears to me that the load address of the hello-world app is not set correctly.
Looking at a dump of the hello_world ELF file shows me that the base address is 0x1c00000.
I then found that the makefile in that directory doesn't support the specifics of the imxQSB, so it defaults to that base address. I think all you need to do is modify examples/standalone/Makefile. The quick change is to set LOAD_ADDR to 0x77800000. I was then able to use tftpboot to launch hello_world successfully.
HTH
Ed
Hi RSmith
Is that loads or loadm command?
Can you please tell me?