Try L2.6.35_11.09.01_ER_source on i.MX35 3Stack board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Try L2.6.35_11.09.01_ER_source on i.MX35 3Stack board

956件の閲覧回数
VincentChou1z
Contributor III

Hi!  I would like to ask whether anyone has experience to build the image for i.MX35 3 Stack board based on L2.6.35_11.09.01_ER_source.  I found the option exists in LTIB but I could not boot the board with the u-boot, kernel and rootfs based on the source.  Any suggestion?

0 件の賞賛
返信
2 返答(返信)

821件の閲覧回数
VincentChou1z
Contributor III

I managed to boot i.MX35 3stack PDK with U-Boot on SD Card and it did go pass the boot stage and hanged at the same place like you came across: Uncompress Linux.  I used 2.6.35 09 source code provided by freescale.  I guess the problem is from the source code itself.  However, I did some research and discovered some people do run 2.6.35 on i.MX35 3Stack board.  How did they do that?

0 件の賞賛
返信

821件の閲覧回数
MartenLootsma1z
Contributor I
One year ago we tried to boot an image of the 2.6.35,without success as well. The difference innour setup is that our bootloader is redboot, but that does not seem to make differences.
0 件の賞賛
返信