Hello, | Working on iMX6 target. I am trying to play a video file using gst pipeline "gst-launch playbin2 uri=file://<full path to sample file>", video and audio is fine until when I try to use trick play mode to seek to stream forward/backward for about xx seconds. What I see in the vpudec and aiurdemux gstreamer plugin code is that some error states like "GST_FLOW_WRONG_STATE" are ignored during trick play mode handling i.e. in gst_vpudec_chain function and in aiurdemux_push_pad_buffer. Please let me know why these event types are ignored or the reason for it. Thank you. |
Steps to reproduce the issue:
1) export GST_DEBUG=*:2
2) gplay <path to seekable video file>
3) Select option 'e' for seek
4) Select seek mode [Fast seek:0, Accurate seek:1]: either '1' or '0'
5) Accurate seek to percentage[0:100] or second [t?]: 10
Seek Output:
seeking: 0:00:59.000000000/0:09:56.459008000
gst_vpudec_show_frame ret=-2
0:00:45.185532613 368 0x7390bc00 WARN vpudec vpudec.c:1569:gst_vpudec_chain: ignoring wrong state: -2
0:00:45.186103280 368 0x766520 WARN aiurdemux aiurdemux.c:3901:aiurdemux_push_pad_buffer: Pad video push error type -2
0:00:45.186224416 368 0x766520 WARN aiurdemux aiurdemux.c:3912:aiurdemux_push_pad_buffer: ignoring GST_FLOW_WRONG_STATE
0:00:45.186763613 368 0x766520 WARN aiurdemux aiurdemux.c:3901:aiurdemux_push_pad_buffer: Pad audio push error type -2
0:00:45.186853810 368 0x766520 WARN aiurdemux aiurdemux.c:3912:aiurdemux_push_pad_buffer: ignoring GST_FLOW_WRONG_STATE
0:00:45.187006734 368 0x766520 WARN aiurdemux aiurdemux.c:3901:aiurdemux_push_pad_buffer: Pad audio push error type -2
0:00:45.187061673 368 0x766520 WARN aiurdemux aiurdemux.c:3912:aiurdemux_push_pad_buffer: ignoring GST_FLOW_WRONG_STATE
0:00:45.187125643 368 0x766520 WARN aiurdemux aiurdemux.c:3901:aiurdemux_push_pad_buffer: Pad video push error type -2
0:00:45.187173037 368 0x766520 WARN aiurdemux aiurdemux.c:3912:aiurdemux_push_pad_buffer: ignoring GST_FLOW_WRONG_STATE
Let me know if it is fine to ignore this state or is there any way to handle it?
Thank you.