Tool for performance analysis for i.MX6Q Sabre Lite Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tool for performance analysis for i.MX6Q Sabre Lite Board

574件の閲覧回数
douglassantos
Contributor I

Hi all,

I'm using the i.MX6Q Sabre Lite Board to test some algorithms and would like to know if there is any tool that can assist me in collecting data, such as processing time and the resources used (CPU, GPU).

Thanks in advance,

Douglas

ラベル(1)
0 件の賞賛
返信
1 返信

400件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Douglas,

I can only recommend that you use the TOP linux command so you can get the information that you are trying to accomplish, here is a link, that can help:

Unbelievable ! 30 Linux TOP Command Examples With Screenshots

For the GPU you can use the VProfiler, that it is a tool from the Vivante SDK,  you can download it from the following link:

I.MX_6_VIVANTE_VDK_150_TOOLS , just a little advise, this is tool it is made for the Freescale BSP since you are using the SABRE Lite board from Nitrogen. You need to check if the GPU it is enable in your kernel.

saludos

0 件の賞賛
返信