Dear I.MX Community experts,
I need to add wic.bmap & wic.bz2 and when I tried to include as below:
IMAGE_FSTYPES = "tar.bz2 ext4 wic.gz wic.bz2 wic.map sdcard.bz2" in "imx/meta-sdk/conf/distro/include/fsl-imx-base.inc" I get the below error, I have attached the log file for your reference to
Error:
====
ERROR: core-image-minimal-1.0-r0 do_image_wic: No kickstart files from WKS_FILES were found: core-image-minimal.imx8mmevk.wks core-image-minimal.wks. Please set WKS_FILE or WKS_FILES appropriately.
ERROR: core-image-minimal-1.0-r0 do_image_wic: Function failed: do_image_wic (log file is located at /home/srinishanmugam/custom_NXP_Tue9_homework/build_core-image-minimal/tmp/work/imx8mmevk-poky-linux/core-image-minimal/1.0-r0/temp/log.do_image_wic.17119)
ERROR: Logfile of failure stored in: /home/srinishanmugam/custom_NXP_Tue9_homework/build_core-image-minimal/tmp/work/imx8mmevk-poky-linux/core-image-minimal/1.0-r0/temp/log.do_image_wic.17119
ERROR: Task (/home/srinishanmugam/custom_NXP_Tue9_homework/sources/poky/meta/recipes-core/images/core-image-minimal.bb:do_image_wic) failed with exit code '1'
Could you please help me how this support can be added?
Kindly do the needful,
Many Thanks in advance
Any news on this? I have the same problem. It seems to be that the custom .wks.in file is not on the search path, but I don't know how/where to add it...
Hello Srinivasan Shanmugam,
There is a patch in the works for adding the WKS files to the i.MX8M EVK to the Community BSP. I believe it should be ready soon.
Regards,
Hi
I am playing rauc and need to modify wks file to add additional partition for rootfs on sdcard.
I add the IMAGE_FSTYPES = "tar.bz2 ext4 wic.gz wic.bz2 wic.map sdcard.bz2" in "imx/meta-sdk/conf/distro/include/fsl-imx-base.inc" I get the similar error (someone posted : https://community.nxp.com/t5/i-MX-Processors/Error-when-building-Yocto-Sumo-with-Bitbake/m-p/879773
/home/yocto/yocto/source/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/dynamic-layers/qt5-layer/recipes-fsl/images/fsl-image-qt5.bb: No IMAGE_CMD defined for IMAGE_FSTYPES entry 'wic.map' - possibly invalid type name or missing support class
ERROR: /home/yocto/yocto/source/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/dynamic-layers/qt5-layer/recipes-fsl/images/fsl-image-qt5-validation-imx.bb: No IMAGE_CMD defined for IMAGE_FSTYPES entry 'wic.map' - possibly invalid type name or missing support class
ERROR: /home/yocto/yocto/source/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-validation-imx.bb: No IMAGE_CMD defined for IMAGE_FSTYPES entry 'wic.map' - possibly invalid type name or missing support class
ERROR: /home/yocto/yocto/source/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-gui.bb: No IMAGE_CMD defined for IMAGE_FSTYPES entry 'wic.map' - possibly invalid type name or missing support class
I am using yocto sumo, L4.14.98-2.0.0_ga
you mentioned that "
There is a patch in the works for adding the WKS files to the i.MX8M EVK to the Community BSP. I believe it should be ready soon.
"
---
where is the patch? and how to fix , thank you.
I posted my all rauc issue at here:
Hi Gusarambula,
Can you share some information regarding this patch, if its ready by now. please share the link.
Regards
Mani
Hi Gusarambula,
How to fix this issue ? , please let me know as i am facing the same error. .. ?
Initialising tasks: 100% |######################################################################################################| Time: 0:00:03
Sstate summary: Wanted 216 Found 206 Missed 10 Current 1497 (95% match, 99% complete)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: agl-image-minimal-1.0-r0 do_image_wic: No kickstart files from WKS_FILES were found: agl-image-minimal.imx8mqevk.wks agl-image-minimal.wks. Please set WKS_FILE or WKS_FILES appropriately.
ERROR: agl-image-minimal-1.0-r0 do_image_wic: Function failed: do_image_wic (log file is located at /home/imx8/workspace_agl/build/tmp/work/imx8mqevk-agl-linux/agl-image-minimal/1.0-r0/temp/log.do_image_wic.9113)
ERROR: Logfile of failure stored in: /home/imx8/workspace_agl/build/tmp/work/imx8mqevk-agl-linux/agl-image-minimal/1.0-r0/temp/log.do_image_wic.9113
ERROR: Task (/home/imx8/workspace_agl/meta-agl/meta-agl-profile-core/recipes-platform/images/agl-image-minimal.bb:do_image_wic) failed with exit code '1'