Thermal measurement uboot IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Thermal measurement uboot IMX6

Jump to solution
828 Views
cblack
Contributor I

I am trying to get an idea of exactly what the temperature routine in u-boot imx is measuring.  It mentions BM_ANADIG_TEMPSENSE0_XXX  registers in the read_cpu_temperature() function.

Is this measuring die temperature? Casing temperature?

thanks

Curt

Labels (2)
0 Kudos
1 Solution
496 Views
igorpadykov
NXP Employee
NXP Employee

Hi Curt

it is measuring die temperature.

Best regards

igor
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
497 Views
igorpadykov
NXP Employee
NXP Employee

Hi Curt

it is measuring die temperature.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos