The problem of porting RTL8723AU on I.MX6Q sabresd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The problem of porting RTL8723AU on I.MX6Q sabresd

623 Views
pengxingwei
Contributor III

hello all,

               I came cross a problem when I ported the wifi  on Android4.3 using the chip of Realtek RTL8723AU(USB)  ,the log of system starting as follows:

     8723au: Unknown symbol cfg80211_scan_done (err 0)

     8723au: Unknown symbol cfg80211_remain_on_channel_expired (err 0)

     8723au: Unknown symbol cfg80211_new_sta (err 0)

     8723au: Unknown symbol cfg80211_disconnected (err 0)

     8723au: Unknown symbol cfg80211_ready_on_channel (err 0)

     8723au: Unknown symbol wiphy_register (err 0)

     8723au: Unknown symbol wiphy_new (err 0)

     8723au: Unknown symbol cfg80211_put_bss (err 0)

     8723au: Unknown symbol cfg80211_roamed (err 0)

     8723au: Unknown symbol cfg80211_ibss_joined (err 0)

     8723au: Unknown symbol cfg80211_michael_mic_failure (err 0)

     8723au: Unknown symbol cfg80211_connect_result (err 0)

     8723au: Unknown symbol wiphy_unregister (err 0)

     8723au: Unknown symbol cfg80211_get_bss (err 0)

     8723au: Unknown symbol __ieee80211_get_channel (err 0)

     8723au: Unknown symbol cfg80211_mgmt_tx_status (err 0)

     8723au: Unknown symbol cfg80211_del_sta (err 0)

     8723au: Unknown symbol cfg80211_rx_mgmt (err 0)

     8723au: Unknown symbol cfg80211_inform_bss_frame (err 0)

     8723au: Unknown symbol ieee80211_frequency_to_channel (err 0)

     8723au: Unknown symbol wiphy_free (err 0)

I need some suggestion about it ? thanks!!

Labels (2)
0 Kudos
1 Reply

383 Views
igorpadykov
NXP Employee
NXP Employee

Hi peng

seems some libraries are missed, one can try to debug it

using app note Using Open Source Debugging Tools for Linux on i.MX Processors

http://www.nxp.com/files/32bit/doc/app_note/AN4553.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos