The problem about IMX6DL GPU when running android

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The problem about IMX6DL GPU when running android

2,144 次查看
pengxingwei
Contributor III

Hi all,

       I develop android_m6.0 on imx6dl sabresd board,when I run a application to dynamic plotting wave by the data thransfering from uart  .But there has waveform caton phenomenon and GPU over drawing,which can discover by the AndroidStudio IDE,How to solve the problem or Is not strong performance of GPU on imx6dl?

标签 (2)
0 项奖励
4 回复数

783 次查看
pengxingwei
Contributor III

The phenomenon as shown above

0 项奖励

783 次查看
pengxingwei
Contributor III

1.png2.png3.png

0 项奖励

783 次查看
igorpadykov
NXP Employee
NXP Employee

Hi peng

one can try to investigate it, if it caused by ddr bandwidth and using mmdc profiling tool

About MMDC Profiling Tool for i.MX6 

or try latest android releases from link

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

783 次查看
pengxingwei
Contributor III

Hi igorpadykov,

                     I did the ddr stress through DDR Stress Test tool,and modified the uboot DCD,but The phenomenon is the same as before,

device-2017-11-10-102454.png

0 项奖励