The preview nosie issue for fsl-yocto-L4.1.15

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The preview nosie issue for fsl-yocto-L4.1.15

422 次查看
jwwang
Contributor I

Hi

Originally I exploit the following gstreamer command to test camera preview for our custom imx6q board, and the result is always OK.

gst-launch-1.0 imxv4l2src device=/dev/video1 ! 'video/x-raw, format=(string)NV12, width=1920, height=1080, framerate=(fraction)30/1' ! imxvideoconvert_g2d rotation=3 ! video/x-raw,format=RGB16,width=1080,height=1920 ! autovideosink

I found that there is noise at the edge of camera preview after updating the yocto freescale code from fsl-yocto-L3.14.28-1.0.1 to fsl-yocto-L4.1.15-1.2.0.

And there is also the same phenomenon on freescale imx6q board (refer to the attached image).

How can I remove this preview noise?

Thank you.

Jw Wang

标签 (1)
0 项奖励
1 回复

341 次查看
jimmychan
NXP TechSupport
NXP TechSupport

please try  ! video/x-raw,width=1920,height=1080 !

0 项奖励