Hi,
I am working on the mx6q_sabrelite board with L3.0.35_4.0.0_130424 release.
When I start the ubuntu_oneiric_4.0.0 system, and run some commands, such as apt-get or others, some kernel panic messages may will be shown, and sometimes the system will hang. More detailed kernel panic messages are shown in the attachments. From these messages, it seems that the memory is not enough(Am I right?). Are there any instructions on how to set the system memory, GPU memory and Framebuffer memory? Any idea and patch about these kernel hang???
Thanks in advance.
Original Attachment has been moved to: kernel-hang-01.zip
Original Attachment has been moved to: kernel-hang-03.zip
Original Attachment has been moved to: kernel-hang-02.zip
I have exactly the same issue with my SabreLite board from element14.
I try different u-boots and kernels - both from Freescale, Timesys and Boundary Devices.
Board hangs or kernel panic during heavy loads - extracting large archives, copying big volumes of data.
I.e. it can easily compile a Linux kernel with -j4, but definitely crash when just unpacking it.
Lowering cpu frequency with powersave governor does not help.
I found only one 100% solution - use "maxcpus=1" in kernel command line.
At the same time it is rock-solid on 3.11-rc1 kernel! - Gentoo "world" rebuild works like a charm.
Hi Steven,
I just ran across this post after Karina's mention.
It seems that you're having some pretty massive failures, which we haven't seen in any image, but that we did see before some critical U-Boot and kernel patches surrounding CPU frequency driver.
Can you forward the output of the 'version' command under U-Boot and the output from /proc/version under Linux?
I'd also be interested in seeing the line of U-Boot banner that lists the CPU information:
CPU: Freescale i.MX6Q rev1.0 at 792 MHz
That will give us a starting point for further investigations.
Hi EricNelson,
Thank you!
The output of /proc/version under Linux is as below
Linux version 3.0.35-2508-g54750ff (trigger@IMX6q-LinuxBSP) (gcc version 4.6.2 2
0110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:
20) ) #1 SMP PREEMPT Wed Jun 19 19:42:45 CST 2013
And the output of version' command under U-Boot is as below,
U-Boot 2009.08 (May 29 2013 - 11:54:13)
And the line of U-Boot banner that lists the CPU information
CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 182
Temperature: 39 C, calibration data 0x5834f569
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock : 528000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Hi Steven,
Alright, this shows that you're running both an old U-Boot and a stock-from-freescale kernel.<br/><br/>
The U-Boot should be fixed first. We just bumped the version that we're shipping and this post gives a download link and instructions on how to upgrade:
http://boundarydevices.com/new-u-boot-version/
There's also a "Getting started guide" for U-Boot on our i.MX6 boards here:
http://boundarydevices.com/u-boot-on-i-mx6/
I suspect that this will solve your issues, since the Freescale U-Boot code base has some issues with DDR timings as discussed in this post:
http://boundarydevices.com/i-mx-6dq-u-boot-updates/
We also recommend that you use our kernel on SABRE Lite. You can get a very recent set of binaries and instructions about how to overlay them onto your Oneiric image from here:
http://boundarydevices.com/modifying-a-linux-image/
If you need to (re)compile the kernel, instructions are here:
http://boundarydevices.com/i-mx6-kernel-l3-0-35_4-0-0/
Finally, if you want to skip the "overlay" processes, we have an image here:
http://boundarydevices.com/freescale-ubuntu-image-with-4-0-0-kernel/
(It contains a recent "u-boot.imx" for SABRE Lite and Nitrogen6X)
Do you see the same errors using the ubuntu image that Boundary Devices provides? I am sure this image is better tested on sabre lite that the one Freescale provides.
Leo
Hi,
Thank you so much!
Would you please tell that where and how can I get ubuntu image that Boundary Devices provides?
Which is the best and the most suitable software(kernel+uboot+ubuntu image) for mx6q_sabrelite board?
Hi Steven,
You can get the latest Ubuntu for SABRE Lite from this post:
http://boundarydevices.com/freescale-ubuntu-image-with-4-0-0-kernel/
You can contact EricNelson to get help with Sabre Lite.
As i know, 4.0.0 supports only TO1.2 imx6q.
Would be better you take the kernel from Boundary Devices.
Hi,
Thanks so much for your kindly reply.
Do you mean that 4.0.0 does not support mx6q_sabrelite??? If not, then which release is best for mx6q_sabrelite.
I have tested L3.0.35_1.1.0_121218 release, but the X window will always hang after start X.
Correct, Freescale does not support BSP for SabreLite. Tested releasse are found on BoundaryDevice website or in case you want the latest patches on that machine, try the Yocto framework.
Leo