The detail fo IO DRV in MMPF0100.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The detail fo IO DRV in MMPF0100.

跳至解决方案
730 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about MMPF0100 datasheet.

Please see Table 138, it shows IO DRV register in address 0x90, but there is no description about this register.

Would you let me know the detail, especially RESETBMCU_DRV?

Actually, I want to judge whether I can use RESETBMCU_DRV bit to control RESTBMCU singnal assert/deassert manually.

Best Regards,

Satoshi Shimoda

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
531 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Basically, in Extended Page 2, most of these registers are used in TEST mode,
and may be marked as reserved. The RESETBMCU_DRV is just for tweaking internal

MOSFET drive parameters, not for asserting / deasserting ; RESETBMCU can't be controlled

manually.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
532 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Basically, in Extended Page 2, most of these registers are used in TEST mode,
and may be marked as reserved. The RESETBMCU_DRV is just for tweaking internal

MOSFET drive parameters, not for asserting / deasserting ; RESETBMCU can't be controlled

manually.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复