Hi everyone!
In imx6sx, I need to use gpio6_io01 for interrupt input in Linux and gpio6_io02 for interrupt input in M4.
However, during the test, it is found that only the last configured IO can respond to the interrupt. If gpio6_IO1 is configured first, and then gpio6_io02 is configured, only the A9 can respond to the interrupt. How to solve this problem?
已解决! 转到解答。
Hi long
since this is combined interrupt, I am afraid it is not possible
to serve it simultaneously by both cores. May be useful to check
GPIO1 interrupts, they provide much more flexibility.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi long
since this is combined interrupt, I am afraid it is not possible
to serve it simultaneously by both cores. May be useful to check
GPIO1 interrupts, they provide much more flexibility.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------