The cameras on the SABRE board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The cameras on the SABRE board

跳至解决方案
1,255 次查看
patcharasirigul
Contributor II

Hello everyone,

I bought the SABRE board coming with the camera like a picture below. I would like to know what the part number of the camera using on the Sabre board is ? or where can I find the camera same this module ?

IMG_1722[1].JPG.jpg

IMG_1721[1].JPG.jpg

thank you so much,

Patchara Sirigulyanon

标签 (2)
0 项奖励
1 解答
657 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Patchara

part numbers are given on link below

Camera modules for i.MX6 Quad SABRE Smart Device Platform (Ref.MCIMX6Q-SDP)

many vendors can offer these modules, for example

www.a-kerr.com.

www.nuhorizons.com

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
1 回复
658 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Patchara

part numbers are given on link below

Camera modules for i.MX6 Quad SABRE Smart Device Platform (Ref.MCIMX6Q-SDP)

many vendors can offer these modules, for example

www.a-kerr.com.

www.nuhorizons.com

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励