The VPU of i.MX6 supports VP8 codec with 1920x1080 resolution.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The VPU of i.MX6 supports VP8 codec with 1920x1080 resolution.

878 Views
kmslove
Contributor III

Hi All.

As you may know, the maximum supported resolution of VP8 codec is 1280x720.

The i.MX6 datasheet shows the following:

MX6_VPU_Spec.png

However, as a result of testing with several files(MKV, WebM), the VP8 codec with 1920x1080 resoltuion was also supported.

I tested video decoding using VPU on android 7.1 and Windows Embedded Compact 2013(WEC 2013) OS.

Use the VPU instead of SW type VP8 codec.

I hope this information will help you.

Have a nice day.

Labels (1)
0 Kudos
Reply
0 Replies