The BT.656 mode of IPU problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The BT.656 mode of IPU problem

629件の閲覧回数
wwfdzh2012
Contributor I

Hi,everyone!

  I still having a problem with The BT.656 mode of I.MX6Q's IPU,.We known, BT.656 mode have a timing reference signal consists of a four word sequence(0xff,0x00,0x00,xy). the timeing reference signal is frame start. frame end, line start,line end.But i found that it is only have three states on the 'xy'  of the  progressive mode according to  the IMX6Q reference manual.In the progressive mode, it can only support: start of active line , end of active line and start of blanking line.It can  only corresponding to my sensor Line Start signal,Line End signal and Frame Start signal.So where is Frame End signal?

Update:

   I had study the BT.656 protocol,and the problem has solved. Thank you.

ラベル(4)
0 件の賞賛
2 返答(返信)

498件の閲覧回数
wwfdzh2012
Contributor I

Nobody?

0 件の賞賛

498件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for bt656, you should refer to the protocol of bt656, which describe very detailed about SAV, EAV.