Tell me how to enable the i.MX8M Quad's micro SD card slot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tell me how to enable the i.MX8M Quad's micro SD card slot

Jump to solution
885 Views
KojiTajima
Contributor II

Hi,

Tell me how to enable the i.MX8M Quad's micro SD card slot.

I used to be able to read a micro SD card, but when I changed some settings from U-Boot,

I couldn't read it anymore.

 

Best regards,

KojiTajima

 

0 Kudos
1 Solution
843 Views
KojiTajima
Contributor II

Hello, TechSupport

Thank you for your reply.

I was able to write the Android image to the microSD safely.

The cause was that u_boot used setenv to set SDIO to the M.2 connector.
By setting the M.2 connector to PCIe, SDIO can now be returned to the SD Card slot and writable.
See "4.4.3 Enabling PCIe on M.2" in UM11483.

 

Thanks,

KojiTajima

View solution in original post

4 Replies
844 Views
KojiTajima
Contributor II

Hello, TechSupport

Thank you for your reply.

I was able to write the Android image to the microSD safely.

The cause was that u_boot used setenv to set SDIO to the M.2 connector.
By setting the M.2 connector to PCIe, SDIO can now be returned to the SD Card slot and writable.
See "4.4.3 Enabling PCIe on M.2" in UM11483.

 

Thanks,

KojiTajima

832 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Good news it works well and thanks a lot for your kindly sharing.

0 Kudos
870 Views
KojiTajima
Contributor II

Hello,

I wanted to try booting an Android that is written on the micro SD card, so I tried to flash the Android image along "Android Quick Start Guide".

    [Android Quick Start Guide]

    File Name: Android_Quick_Start_Guide.pdf

    Document Number: AQSUG

    Rev. O8.1.0_1.3.0_8M, 04/2018

But I couldn't flash the Android image to the micro SD card.

 

I did the work as described in "3.3 Flashing board images" in the Android Quick Start Guide.

    - Copy only the specified 6 files into the specified directory.

    - I'm using a 32GB microSD card, so copy partition-table-28GB.img and rename it to partition-table.img.

    - SW802 can be set to 1: OFF and 2: ON.

    - Power on the board.

    - Connect to PC's USB 3.0 port with a USB type-c cable.

    - Insert the micro SD card into the slot after turning on the board.

    - I double-clicked the mfgtool2-android-mx8mq-evk-sd.vbs file and MFG Tool started.

I pressed the Start button here, but the tool got stuck in the attached PNG image.

 

Is the micro SD card not recognized?

Please tell me what is wrong or missing with the procedure.

 

Best Regards,

KojiTajima

MFGTool_is_stuck.png

0 Kudos
853 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using NXP i.MX8MQ EVK board? Which version board are you using? B3,B4 or A1?

0 Kudos