Hi
I try to modify tvp5150.c for i.mx6 board.The input is PAL video source.
The serial port print the message as follow.
TVP5150 io_init
tvp5150_probe:tvp5150 probe i2c address is 0x5D
TVP5150 Chip version = 0x04
type is 2 (expect 2)
num ioctls is 13
In MVC: mxc_v4l2_master_attach
slave.name = tvp5150
master.name = mxc_v4l2_cap1
sdata->csi = 0
cam->csi = 1
tvp5150 mxc_v4l2_master_attach: csi doesn't match
In MVC: mxc_v4l2_master_attach
slave.name = tvp5150
master.name = mxc_v4l2_cap0
sdata->csi = 0
cam->csi = 0
tvp5150 mxc_v4l2_master_attach: csi does match
tvp5150 mxc_v4l2_master_attach type is 2
PAL video source.
tvp5150 mxc_v4l2_master_attach attach___attach___attach
tvp5150 v4l2_int_device_register succeed.
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
When I execute the test command ./mxc_v4l2_tvin.out -ow 720 -oh 480 -ol 10 -ot 20 -f YU12 in linux.
It occurs the errors as follow and can't display on screen.
root@freescale /unit_tests$
< 160 -oh 160 -ot 20 -ol 20 -r 0 -t 50 -d 0 -fg -fr 30
start_________start_________start_________start_________start_________start_________start
tvp5150 mxc_v4l_open type is 2 (expect 2)
end___________end___________end___________end___________end___________end___________end
PAL video source.
success________success_________success_________success_________success_________success_________success
tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
TV decoder chip is tvp5150tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
PAL video source.
tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
In mxc_v4l2_s_std ff
tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
PAL video source.
imx-ipuv3 imx-ipuv3.0: Unsupported CCIR656 interlaced video mode
tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
VIDIOC_G_FMT failed
tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
driver=mxc_vout, card=DISP3 FG, bmxc_v4l2_output mxc_v4l2_output.0: Enable deinterlace BT.
us=, version=0x00000000, capabilities=0x04000002
fmt RGB565: fourcc = 0x50424752
fmt BGR24: fourcc = 0x33524742
fmt RGB24: fourcc = 0x33424752
fmt RGB32: fourcc = 0x34424752
fmt BGR32: foutvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
rcc = 0x34524742
fmt NV12: fourctvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
c = 0x3231564e
fmt UYVY: fourcc tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
= 0x59565955
fmt YUYV: fourcc = tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
0x56595559
fmt YUV422 planar: fotvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
urcc = 0x50323234
fmt YUV444: fotvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
urcc = 0x34343459
fmt YUV420: fotvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
urcc = 0x32315559
fmt TILED NV12PAL video source.
P: fourcc = 0x50564e54
fmt TILEDtvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
NV12F: fourcc = 0x46564e54
fmt YUV444 planar: fourcc = 0x50343434
start time = 330 s, 691641 us
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
VIDIOC_DQBUF failed.
tvp5150 do_ioctl___do_ioctl___do_ioctl___do_ioctl
tvp5150 close___close___close___close
root@freescale /unit_tests$
The ioctl_g_ifparm as follow:
static int ioctl_g_ifparm(struct v4l2_int_device *s, struct v4l2_ifparm *p)
{
dev_dbg(&tvp5150_data.i2c_client->dev, "In tvp5150:ioctl_g_ifparm\n");
if (s == NULL) {
pr_err(" ERROR!! no slave device set!\n");
return -1;
}
/* Initialize structure to 0s then set any non-0 values. */
memset(p, 0, sizeof(*p));
p->if_type = V4L2_IF_TYPE_BT656; /* This is the only possibility. */
p->u.bt656.mode = V4L2_IF_TYPE_BT656_MODE_NOBT_8BIT;
p->u.bt656.nobt_hs_inv = 1;
p->u.bt656.bt_sync_correct = 1;
/* TVP5150 has a dedicated clock so no clock settings needed. */
return 0;
}
Who can help to fix the problem?
Thanks.
已解决! 转到解答。
Looks like your driver has several setup problems, first of all this one:
Unsupported CCIR656 interlaced video mode
Means your tvp5150 driver does not respond with proper format caps inside its ioctl_g_fmt_cap. Since you are using PAL signal you have to fill v4l2_format structure in that ioctl with proper format (720x625 in your case, refer to ipu_capture.c). This is most likely sole reason of your problem. Also double check your platform code (are csi and ipu fields filled properly for your physical connection to TVP5150 from mx6, did you set up pads correctly?). Make sure TVP5150 is sending out bt656 data and not raw 4:2:2.
Looks like your driver has several setup problems, first of all this one:
Unsupported CCIR656 interlaced video mode
Means your tvp5150 driver does not respond with proper format caps inside its ioctl_g_fmt_cap. Since you are using PAL signal you have to fill v4l2_format structure in that ioctl with proper format (720x625 in your case, refer to ipu_capture.c). This is most likely sole reason of your problem. Also double check your platform code (are csi and ipu fields filled properly for your physical connection to TVP5150 from mx6, did you set up pads correctly?). Make sure TVP5150 is sending out bt656 data and not raw 4:2:2.
The TVin function was verified with adv7180 on L3.0.35_4.0.0 BSP, so for your TVP5150, you should make sure the output from this tvin chip is BT656 PAL or NTSC, included EAV/SAV data on data bus. Then no code modification was needed in other IPU driver code.
By the way, your "ioctl_g_ifparm" setting is OK, please also make sure in the sensor probe function, such as adv7180_probe, there is the followed code:
adv7180_data.sen.pix.pixelformat = V4L2_PIX_FMT_UYVY; /* YUV422 */
adv7180_data.sen.pix.priv = 1; /* 1 is used to indicate TV in */
adv7180_data.sen.on = true;
For the test application, you can just run as followed:
./mxc_v4l2_tvin.out -ow 720 -oh 480 -ot 10 -ol 10
Thanks, Li. I haved checked my tvp5150.c file again,there is no problem.
I use the linux kernel is the kenel_imx of i.MX 6 Android R13.4.1,does the kernel support the adv7180,shall I get the newest kernel of i.mx6?