TJA1100 PHY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1100 PHY

1,132件の閲覧回数
ramijajo
Contributor I

Hello everyone,

i am trying to program the TJA1100 PHY for BroadR-Reach Automotiv Ethernet with a STM32F407 µC. The PHY does not send anything over the twisted pair cable.

I read the value of the PHY registers:

Basic control register: 0x2100
Basic status register: 0x1E1
PHY identifier register1: 0x180
PHY identifier register2: 0xDC48
Extended status register: 0x80
Extended control register: 0x9802
Configuration register1: 0x5A11
Configuration register2: 0x2245
Symbol error conter register2: 0x00
Interrupt status register: 0x00
Interrupt enable register: 0x8000
Communication status register: 0x6004
General status register: 0xC000
External status register: 0x00
Link fail counter register: 0x00

Are the settings correct?
What changes should i do?

Thank you in advance.

Best regards

0 件の賞賛
1 返信

578件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rami

unfortunately I am not aware of tja1100 driver, but one can check datasheet and common steps

http://cache.nxp.com/documents/data_sheet/TJA1100.pdf 

TJA1100 in imx6 with Managed mode 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛