We have a composite video decoder chip (TW9912) that can produce either Interlaced or Progressive bt.656 video, fed into CSI0.
In our application we do this:
fmt.fmt.pix.field = V4L2_FIELD_INTERLACED;
ioctl(Fd_v4l_camera, VIDIOC_S_FMT, &fmt)
... and this works great when the video chip is in Interlaced mode; there's a reasonable but interlaced picture.
Now if we change the video chip to Progressive mode and also do this:
fmt.fmt.pix.field = V4L2_FIELD_NONE; // according to V4L2, this means Progressive
ioctl(Fd_v4l_camera, VIDIOC_S_FMT, &fmt)
... this gives no picture at all, though we can see data entering the CSI port from the video chip. This is the only change we made to our app. The drivers give no error, and if we read back the fmt using VIDIOC_G_FMT we see the correct value for fmt.fmt.pix.field (it is value 1).
Could someone please advise what we must do to configure the iMX to interface with a Progressive bt.656 signal.
Many thanks
已解决! 转到解答。
You can try this:
change
csi_param.clk_mode = IPU_CSI_CLK_MODE_CCIR656_INTERLACED;
for
csi_param.clk_mode = IPU_CSI_CLK_MODE_CCIR656_PROGRESSIVE;(mxc_v4l2_capture.c mxc_v4l2_s_param)
hi Paul Hottell
you can write your own tw9912.c according adv7180.c in \kernel\linux-2.6.35\drivers\media\video\mxc\capture
it is not as difficult as you think。
you can communite to your chip supporter to get the register table
Thanks for the good advice to mod mxc_v4l2_capture.
We now have an excellent progressive picture from an interlaced composite source - this gets around the deinterlacer of the iMX only being on the 'back end'. The only thing is we find we are getting 50 full *frames* reported per second from a PAL source, we expect 25.
Our camera thread is like most others where it just blocks to dequeue a camera buffer, and we see 50 of these per second. As a temp workaround we discard alternate buffer events to bring it back to 25, but I guess there is a nicer way.
When we were originally using interlaced input, we had 25 FPS, the only change made was the simple change that was recommended for getting progressive mode, and now it's 50.
Maybe someone knows of something else we need to change to get progressive back down to 25 FPS? Many thanks.
Hi Steve,
Could you tell us on which kind of i.MX processor and which SW version you succeeded in using 576p video decoded by the TW9912 ?
We are facing the same kind of problem on i.MX6Dual with Linux 3.0.35_4.0.0 decoded by an ADV7280 chip (which seems a competitor of the TW9912 as it can also convert PAL or NTSC interlaced flow to progressive at 50 fps for PAL or 60 fps for NTSC on BT656).
If anybody else succeeded in reading PAL progressive video on BT656 on i.MX6, we would be interested as we didn't succeed (yet) and we wonder if anybody already did it on i.MX6.
Regards,
Hervé.
Hi Zhanxiaozhang,
So you have first used an external chip (TW9912) to deinterlace on i.MX6, and - as you were not satisfied by the resulting quality (rolling every 10s) - you changed the deinterlacing principle by making it done by the i.MX6 internal VDIC. If this is what really happened, I'm quite worried because we've done the same tests the other side:
Could you just answer the following questions to help us (and other people reading this post):
Thanks a lot for your help.
Regards,
Hervé.
------------it rolling infitely (per 10s)
hi Steve Green
recently i am working on tw9912,but my Manufacture did not give me any inux driver,so it is very difficult for me to write the code without a reference,can u share your code ?
thanks