Hi Community,
I am using the Ubuntu based Desktop (BSP 5.10.72-2.2.0) on iMX8M Plus, but the IP addresses that the Ethernet interfaces obtain are weird :
eth0: flags=-28605<UP,BROADCAST,RUNNING,MULTICAST,DYNAMIC> mtu 1500
inet 169.254.83.180 netmask 255.255.0.0 broadcast 169.254.255.255
inet6 fe80::204:9fff:fe06:c9f8 prefixlen 64 scopeid 0x20<link>
ether 00:04:9f:06:c9:f8 txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 49 bytes 8556 (8.5 KB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
eth1: flags=-28605<UP,BROADCAST,RUNNING,MULTICAST,DYNAMIC> mtu 1500
inet 169.254.186.180 netmask 255.255.0.0 broadcast 169.254.255.255
inet6 fe80::204:9fff:fe06:c9f9 prefixlen 64 scopeid 0x20<link>
ether 00:04:9f:06:c9:f9 txqueuelen 1000 (Ethernet)
RX packets 4 bytes 536 (536.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 55 bytes 10210 (10.2 KB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
device interrupt 52
or
eth1: flags=-28605<UP,BROADCAST,RUNNING,MULTICAST,DYNAMIC> mtu 1500
inet 169.254.186.180 netmask 255.255.0.0 broadcast 169.254.255.255
inet6 fe80::204:9fff:fe06:c9f9 prefixlen 64 scopeid 0x20<link>
ether 00:04:9f:06:c9:f9 txqueuelen 1000 (Ethernet)
RX packets 4 bytes 536 (536.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 55 bytes 10210 (10.2 KB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
device interrupt 52
Meanwhile, the gateway/router only attributes 192.168.1.x.
Does anyone observe same issue ?
Best Regards,
K
Hi @Bio_TICFSL ,
With the same Ethernet connection, my laptop has valid LAN address.
I also configured so that the router attributed a static IP addresses for the MACs of iMX8MP-EVK, but it still got weird IP addresses :
Meanwhile, it worked well when I connected the EVK into my laptop with DHCP server installed, expected IP address was attributed.