Greetings all,
Im having a bunch of performance issues using recent 3.x linux kernels (slow uSD, USB, linuxfb, etc performance).
It also appears cpufreq, powersaving, etc functions are not availiable.
Is there any Freescale support/maintenance of the iMX28 in the 3.x kernels, or would i be better off moving back to 2.6.35 with related Freescale patches?
Thanks in advance,
Mark,
Which kernel version did you use? It would be nice if you could report the issues you noticed in the linux-arm-kernel mailing list, so that people could be aware of them and eventually fix them.
Hi Mark
I think you are right, since officially supported only releases located
on Freescale i.MX product web pages, like below
i.MX28 Evaluation Kit|Freescale
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------