Starting Android Linux kernel but not Android framework

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Starting Android Linux kernel but not Android framework

Jump to solution
2,184 Views
Goi
Contributor II

Hi,

I have an i.MX53 QSB with Gingerbread, and I'm wondering if it's possible start just the Linux kernel and not the Android framework? I would like to be able to get shell access (via UART or ADB) and play around with some things before starting the full Android OS.

Thanks!

Labels (3)
1 Solution
1,977 Views
xinyu_chen
NXP Employee
NXP Employee

You can remove the "class_start main" in the init.rc

View solution in original post

1 Reply
1,978 Views
xinyu_chen
NXP Employee
NXP Employee

You can remove the "class_start main" in the init.rc