Speed to ethernet port for getting video from 4 IP cameras?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Speed to ethernet port for getting video from 4 IP cameras?

835 次查看
vinayakaghor
Contributor I

Hello,

For getting video from 4 Ip cameras , what should be speed of ethernet port of processor? 100 Mbps will be sufficient?

Regards,

Vinayak

0 项奖励
回复
3 回复数

650 次查看
igorpadykov
NXP Employee
NXP Employee

Hi vinayak

this depends on resolutions@fps and as raw estimation one can consider

100 Mbps/4=25Mbps (~3MB/s) per camera, that results to VGA@10fps

In general this performance corresponds to what is practically

achieved with i.MX27 IP Camera Design

http://www.freescale.com/files/32bit/doc/fact_sheet/IPCAMAZPTNRFS.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

650 次查看
vinayakaghor
Contributor I

Hello,

Basically I want to get H.264 compressed data from 4 Ip cameras with ethernet cable of 100Mbps "each". Then I want this traffic on single port using switch then as per calculations if  use below specs:

"

HD 1080P/2MP30 fpsH.264Expect 4 Mbps per camera

"

That 5th port of 100Mbps would suffice? But Will iMx6 be able to process all 4 videos at same time?

Regards,

Vinayak

0 项奖励
回复

650 次查看
igorpadykov
NXP Employee
NXP Employee

470 Mbps is max. i.MX6 ENET performance (ERR004512)

HD 1080P/2MP 30 fps => 60MP/s, assuming 1 byte/pixel =>

480 Mbps

0 项奖励
回复