Hello,
Need to perform a 720p image rotation 1 deg @15fps minimum.
Looking at the latest i.MX Linux User's Guide , Rev. L3.14.52_1.1.0p-ga, 12/2015, there is a GStreamer v1.0 element "imxvideoconvert" which can perform rotation. The rotation value eludes to 90, 180, 270 rotation only.
gst-launch-1.0 videotestsrc ! imxvideoconvert_{xxx} rotation=2 ! ximagesink display=:0
Is there a hardware method to do this kind of image rotation, or is it best left for a custom GPU function?
Thank you in advance,
Scott
Thanks for the quick response. I was under the impression that the GPU and IPU can only do image rotation 90 degs at a time. I need to perform a 360 deg rotation, 1 deg at a time at 15 fps minimum. Did this change in the SoloX GPU? Thought the GPU was the same as the other i.MX6.