Hi There,
I have a custom board of and soloX and a SoloX sabre SD, both have the has a similar uboot build with only uart1 and the qspi enable. I have tried booting a simple MQX "helloworld" on my custom board and it failed. I am puzzle by this situation, because i have the same uboot setup for my SoloX sabre SD, and it work fined.
i found that the different between my custom board and the SoloX sabre SD is on the accessing the RDC register. RDC register access totally failed on my custom board.
this link below might shed some thing about the nature of my problem:
https://community.nxp.com/message/861365?commentID=861365#comment-861365
Custom Board(1525):
=> md 0x20FC204
020fc204: <<--Uboot hangs
SoloX sabre SD (1533):
Word 0x00000000: 00000000
=> md 0x20FC204
020fc204: 00000000 00000000 00000000 00000000 ................
020fc214: 00000000 00000000 00000000 00000000 ................
020fc224: 00000000 00000000 00000000 00000000 ................
020fc234: 00000000 00000000 00000000 00000000 ................
020fc244: 00000000 00000000 00000000 00000000 ................
020fc254: 00000000 00000000 00000000 00000000 ................
020fc264: 00000000 00000000 00000000 00000000 ................
020fc274: 00000000 00000000 00000000 00000000 ................
020fc284: 00000000 00000000 00000000 00000000 ................
020fc294: 00000000 00000000 00000000 00000000 ................
020fc2a4: 00000000 00000000 00000000 00000000 ................
020fc2b4: 00000000 00000000 00000000 00000000 ................
020fc2c4: 00000000 00000000 00000000 00000000 ................
020fc2d4: 00000000 00000000 00000000 00000000 ................
020fc2e4: 00000000 00000000 00000000 00000000 ................
020fc2f4: 00000000 00000000 00000000 00000000 ................
=> <<-- Uboot ok
Hope that anyonecould assist me, Thank you.
Best Regards,
Nidhal
Btw , Check M4 link file provided
It seems different from the one expected
M4 build result is different from the provided m4_bin.h content
Seem to be relative TCM-L adress , may be aliased ...? 0x0000.0000 in LD file vs 0x1FFF8000 in the header file
Hi Nidhal
please check i.MX6SX Errata
http://cache.freescale.com/files/32bit/doc/errata/IMX6SXCE.pdf
Best regards
igor
Hi Nidhal
youa are right, for RDC issues reason may be Errata #: ERR009572,
to check relevant fuse you can create service request to obtain additional
info about PCIe_DISABLE address.
How to create service request :
https://community.freescale.com/docs/DOC-329745
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------