Silex Module in iMX6 SABRESD board not working with Android version 5.0 and above

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Silex Module in iMX6 SABRESD board not working with Android version 5.0 and above

605件の閲覧回数
senthilkumar_s1
Contributor II

Dear All,

On the board iMX6dq SABRESD, we have flashed the latest Android 5.0 source code downloaded from Freescale.com, but am unable to enable Bluetooth. Kindly provide complete solutions so as to how the bluetooth can be enabled and perform all the functionalities of it..

Below attached is the screenshot of my present state of the SABRESD board highlighting the disabled state of BLuetooth.

Thanks

ラベル(2)
0 件の賞賛
1 返信

416件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Two comments.

1) Have you seen this thread? https://community.freescale.com/docs/DOC-94235

2) Android has removed the support for Silex and now Murata Wifi modules are supported out of the box. Check release notes of your particular Android BSP

Luis

0 件の賞賛