Silex Module in iMX6 SABRESD board not working with Android version 5.0 and above

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Silex Module in iMX6 SABRESD board not working with Android version 5.0 and above

1,372 Views
senthilkumar_s1
Contributor II

Dear All,

On the board iMX6dq SABRESD, we have flashed the latest Android 5.0 source code downloaded from Freescale.com, but am unable to enable Bluetooth. Kindly provide complete solutions so as to how the bluetooth can be enabled and perform all the functionalities of it..

Below attached is the screenshot of my present state of the SABRESD board highlighting the disabled state of BLuetooth.

Thanks

Labels (2)
0 Kudos
Reply
1 Reply

1,183 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Two comments.

1) Have you seen this thread? https://community.freescale.com/docs/DOC-94235

2) Android has removed the support for Silex and now Murata Wifi modules are supported out of the box. Check release notes of your particular Android BSP

Luis

0 Kudos
Reply