Shematics on MCIMX6Q-SD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Shematics on MCIMX6Q-SD

Jump to solution
2,040 Views
christophe
Contributor V

Hi,

We don't have Allegro software and consequently we can't import .brd file on our shematics software (Altium).

Could be possible someone from Freescale send us schematics for the Sabre MCIMX6Q-SD, exported into a 16.2 version (version after 16.2 are not supported on Altium).

Thanks,

CC.


1 Solution
1,200 Views
Yuri
NXP Employee
NXP Employee

The file ORCAD_16_2.zip was from Mark.
I can read it in OrCad 9.1.

Enclosed is the same file, saved in OrCad 7_2 format.

View solution in original post

0 Kudos
11 Replies
1,200 Views
sergeyprilepin
Contributor I


Hi Yuri,

can You give the layout file of MCIMX6Q-SD in ORCAD v. 16.2 format?
We looking for making device based on i.MX6 processor, and I need to have a reference design.

Thanks at any case.

0 Kudos
1,200 Views
Yuri
NXP Employee
NXP Employee

Perhaps the following helps (layout file in text format)

https://community.freescale.com/message/317524#317524

0 Kudos
1,200 Views
sergeyprilepin
Contributor I

Hi, Yuri,

I have a sily question about SABRE schematic: there are a lot of solder shorts and resistors with zero resistance.

Шы ше result of ALLEGRO back annotation from PCB Editor to Schematic Editor?

Thanks at any case!

0 Kudos
1,200 Views
Yuri
NXP Employee
NXP Employee

I am not a member of the SABRE design team, but - my opinion -  solder shorts and resistors with zero resistance are not result
of back annotation. Usually they are inserted in schematic design stage as test / measurements points.

0 Kudos
1,200 Views
sreekn
Contributor I

Hi,

I am trying to open the reference design, "SCH-27417_C3.DSN" for i.MX6 Dual lite in OrCAD 9.1, however it returns "an unsupported file format" error. Any hope to get the file compatible for OrCAD 9.1 version ? Thanks in advance.

0 Kudos
1,200 Views
Yuri
NXP Employee
NXP Employee

Please try the enclosed.

1,200 Views
christophe
Contributor V

Hi Yuri,

What do you mean ?

In the Sabre box, the sd card contains only android stuff. And on the Freescale's site, design files are with Allegro format.

Rgds,

Christophe.

0 Kudos
1,200 Views
christophe
Contributor V

Sorry, i haven't seen the joint file. I try it.

0 Kudos
1,200 Views
christophe
Contributor V

Hi Yuri,

No, it doesn't work. Now, i remember: it was the same thing with the IMX53QSB. The only way is to export the schematics with Allegro/Orcad under a 16.2 version. Ask to Mark Middleton, he's the designer of the board.

Rgds,

Christophe.

0 Kudos
1,201 Views
Yuri
NXP Employee
NXP Employee

The file ORCAD_16_2.zip was from Mark.
I can read it in OrCad 9.1.

Enclosed is the same file, saved in OrCad 7_2 format.

0 Kudos
1,200 Views
christophe
Contributor V

Hi Yuri,

It works fine with Altium.

Thank you.

Rgds,

Christophe.

0 Kudos