Greetings,
My team is utilizing NXP's imxrt1064 microcontroller and Murata's 1ZM bluetooth/wifi radio in our product. We would like to put the 1ZM to sleep when it is not being used. I found the application note "Enabling Bluetooth Deep-sleep with NXP Bluetooth UART Driver" and used it as a starting point.
I believe I am able to put the 1ZM to sleep but I am having issues waking it up. The following is pseudo code for what I am doing.
Sleep scenario
-send hci command to enable deep sleep mode
tx message : 01 23 FC 04 02 00 00 00
rx message : 04 FF 03 23 02 00
- Verify that the rx line is idle
- send the break on character
LPUART2->CTRL |= LPUART_CTRL_SBK_MASK;
Wake up Scenario:
- send break off character ( this is done by inverting the tx pin)
LPUART2->CTRL |= LPUART_CTRL_TXINV_MASK;
-delay 300ms
-disable sending the "BREAK ON" character and invert tx pin
LPUART_BASE->CTRL &= ~(LPUART_CTRL_SBK_MASK | LPUART_CTRL_TXINV_MASK);
-send hci command to disable deep sleep mode
tx message : 01 23 FC 04 02 00 00 00
rx message : 04 10 01 22
I believe the rx message for disabling deep sleep mode is an error message,
HCI_EVENT_HARDWARE_ERROR and the actual error is
ERROR_CODE_LMP_RESPONSE_TIMEOUT_LL_RESPONSE_TIMEOUT. Am I missing anything? Are there any flaws in my pseudo code? The 1ZM has a device wake GPIO pin(GPIO12), should that pin be in a specific state during this process?
已解决! 转到解答。
I fixed the problem I was having. For sending the Break On Signal, I just needed to do the following: LPUART2->CTRL |= LPUART_CTRL_TXINV_MASK. Then to disable it do the following LPUART_BASE->CTRL &= ~LPUART_CTRL_TXINV_MASK.
I fixed the problem I was having. For sending the Break On Signal, I just needed to do the following: LPUART2->CTRL |= LPUART_CTRL_TXINV_MASK. Then to disable it do the following LPUART_BASE->CTRL &= ~LPUART_CTRL_TXINV_MASK.
Hello,
Thank you in advance for contacting NXP support.
We have a User Guide for Bluetooth that you will find useful in order to solve this problem, this user guide explain sleep and wake up command, I don’t know if you have access to this document. This is located under Secure Files section on the 88W8987. Please let me know if you have access to this documentation.
Hello,
If you are not able to see any documentation is necessary to request special access to this. I will recommend to contact your NXP distributor so they can provide the access to this documentation. Please let me know if there is anything else where we can help you.