Setting SDRAM clock on i.mxRT1176

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Setting SDRAM clock on i.mxRT1176

跳至解决方案
980 次查看
revolutesea
Contributor II

Hi,

Currently, we use the i.mxRT1172 for LCD project. I use emwin for SDK example code.

As I know SDK's emwin project setting the max SDRAM bandwidth of RT1170 is 200x2 = 400 MB/s,

However, we need to change the clock from SDRAM setting form 200MHz to 166MH, base on our SDRAM's spec.

Could you provide the example for 166MHz SDRAM or clearfy why I am unable to reduce the SDRAM clock?

The following is my dcd setting

#include "dcd.h"

/* Component ID definition, used by tools. */
#ifndef FSL_COMPONENT_ID
#define FSL_COMPONENT_ID "platform.drivers.xip_board"
#endif

#if defined(XIP_BOOT_HEADER_ENABLE) && (XIP_BOOT_HEADER_ENABLE == 1)
#if defined(XIP_BOOT_HEADER_DCD_ENABLE) && (XIP_BOOT_HEADER_DCD_ENABLE == 1)
#if defined(__CC_ARM) || defined(__ARMCC_VERSION) || defined(__GNUC__)
__attribute__((section(".boot_hdr.dcd_data"), used))
#elif defined(__ICCARM__)
#pragma location = ".boot_hdr.dcd_data"
#endif

/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!GlobalInfo
product: DCDx V2.0
processor: MIMXRT1176xxxxx
package_id: MIMXRT1176DVMAA
mcu_data: ksdk2_0
processor_version: 0.0.0
output_format: c_array
* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/
/* COMMENTS BELOW ARE USED AS SETTINGS FOR DCD DATA */
const uint8_t dcd_data[] = {
/* HEADER */
/* Tag */
0xD2,
/* Image Length */
0x05, 0x08,
/* Version */
0x41,

/* COMMANDS */

/* group: 'Imported Commands' */
/* #1.1-139, command header bytes for merged 'Write - value' command */
0xCC, 0x04, 0x5C, 0x04,
/* #1.1, command: write_value, address: CCM_CLOCK_ROOT4_CONTROL, value: 0x703, size: 4 */
0x40, 0xCC, 0x02, 0x00, 0x00, 0x00, 0x07, 0x03,//0x09,//0x07,//0x03,
/* #1.2, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_00, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x10, 0x00, 0x00, 0x00, 0x00,
/* #1.3, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_01, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x14, 0x00, 0x00, 0x00, 0x00,
/* #1.4, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_02, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x18, 0x00, 0x00, 0x00, 0x00,
/* #1.5, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_03, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x1C, 0x00, 0x00, 0x00, 0x00,
/* #1.6, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_04, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x20, 0x00, 0x00, 0x00, 0x00,
/* #1.7, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_05, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x24, 0x00, 0x00, 0x00, 0x00,
/* #1.8, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_06, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x28, 0x00, 0x00, 0x00, 0x00,
/* #1.9, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_07, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x2C, 0x00, 0x00, 0x00, 0x00,
/* #1.10, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_08, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x30, 0x00, 0x00, 0x00, 0x00,
/* #1.11, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_09, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x34, 0x00, 0x00, 0x00, 0x00,
/* #1.12, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_10, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x38, 0x00, 0x00, 0x00, 0x00,
/* #1.13, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_11, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x3C, 0x00, 0x00, 0x00, 0x00,
/* #1.14, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_12, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x40, 0x00, 0x00, 0x00, 0x00,
/* #1.15, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_13, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x44, 0x00, 0x00, 0x00, 0x00,
/* #1.16, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_14, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x48, 0x00, 0x00, 0x00, 0x00,
/* #1.17, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_15, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x4C, 0x00, 0x00, 0x00, 0x00,
/* #1.18, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_16, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x50, 0x00, 0x00, 0x00, 0x00,
/* #1.19, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_17, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x54, 0x00, 0x00, 0x00, 0x00,
/* #1.20, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_18, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x58, 0x00, 0x00, 0x00, 0x00,
/* #1.21, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_19, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x5C, 0x00, 0x00, 0x00, 0x00,
/* #1.22, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_20, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x60, 0x00, 0x00, 0x00, 0x00,
/* #1.23, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_21, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x64, 0x00, 0x00, 0x00, 0x00,
/* #1.24, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_22, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x68, 0x00, 0x00, 0x00, 0x00,
/* #1.25, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_23, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x6C, 0x00, 0x00, 0x00, 0x00,
/* #1.26, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_24, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x70, 0x00, 0x00, 0x00, 0x00,
/* #1.27, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_25, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x74, 0x00, 0x00, 0x00, 0x00,
/* #1.28, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_26, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x78, 0x00, 0x00, 0x00, 0x00,
/* #1.29, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_27, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x7C, 0x00, 0x00, 0x00, 0x00,
/* #1.30, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_28, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x80, 0x00, 0x00, 0x00, 0x00,
/* #1.31, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_29, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x84, 0x00, 0x00, 0x00, 0x00,
/* #1.32, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_30, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x88, 0x00, 0x00, 0x00, 0x00,
/* #1.33, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_31, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x8C, 0x00, 0x00, 0x00, 0x00,
/* #1.34, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_32, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x90, 0x00, 0x00, 0x00, 0x00,
/* #1.35, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_33, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x94, 0x00, 0x00, 0x00, 0x00,
/* #1.36, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_34, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x98, 0x00, 0x00, 0x00, 0x00,
/* #1.37, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_35, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0x9C, 0x00, 0x00, 0x00, 0x00,
/* #1.38, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_36, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xA0, 0x00, 0x00, 0x00, 0x00,
/* #1.39, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_37, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xA4, 0x00, 0x00, 0x00, 0x00,
/* #1.40, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_38, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xA8, 0x00, 0x00, 0x00, 0x00,
/* #1.41, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_39, value: 0x10, size: 4 */
0x40, 0x0E, 0x80, 0xAC, 0x00, 0x00, 0x00, 0x10,
/* #1.42, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_40, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xB0, 0x00, 0x00, 0x00, 0x00,
/* #1.43, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_41, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xB4, 0x00, 0x00, 0x00, 0x00,
/* #1.44, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_00, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xB8, 0x00, 0x00, 0x00, 0x00,
/* #1.45, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_01, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xBC, 0x00, 0x00, 0x00, 0x00,
/* #1.46, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_02, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xC0, 0x00, 0x00, 0x00, 0x00,
/* #1.47, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_03, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xC4, 0x00, 0x00, 0x00, 0x00,
/* #1.48, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_04, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xC8, 0x00, 0x00, 0x00, 0x00,
/* #1.49, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_05, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xCC, 0x00, 0x00, 0x00, 0x00,
/* #1.50, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_06, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xD0, 0x00, 0x00, 0x00, 0x00,
/* #1.51, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_07, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xD4, 0x00, 0x00, 0x00, 0x00,
/* #1.52, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_08, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xD8, 0x00, 0x00, 0x00, 0x00,
/* #1.53, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_09, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xDC, 0x00, 0x00, 0x00, 0x00,
/* #1.54, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_10, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xE0, 0x00, 0x00, 0x00, 0x00,
/* #1.55, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_11, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xE4, 0x00, 0x00, 0x00, 0x00,
/* #1.56, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_12, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xE8, 0x00, 0x00, 0x00, 0x00,
/* #1.57, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_13, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xEC, 0x00, 0x00, 0x00, 0x00,
/* #1.58, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_14, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xF0, 0x00, 0x00, 0x00, 0x00,
/* #1.59, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_15, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xF4, 0x00, 0x00, 0x00, 0x00,
/* #1.60, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_16, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xF8, 0x00, 0x00, 0x00, 0x00,
/* #1.61, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_17, value: 0x00, size: 4 */
0x40, 0x0E, 0x80, 0xFC, 0x00, 0x00, 0x00, 0x00,
/* #1.62, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_18, value: 0x00, size: 4 */
0x40, 0x0E, 0x81, 0x00, 0x00, 0x00, 0x00, 0x00,
/* #1.63, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_19, value: 0x00, size: 4 */
0x40, 0x0E, 0x81, 0x04, 0x00, 0x00, 0x00, 0x00,
/* #1.64, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_20, value: 0x00, size: 4 */
0x40, 0x0E, 0x81, 0x08, 0x00, 0x00, 0x00, 0x00,
/* #1.65, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_00, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x54, 0x00, 0x00, 0x00, 0x08,
/* #1.66, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_01, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x58, 0x00, 0x00, 0x00, 0x08,
/* #1.67, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_02, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x5C, 0x00, 0x00, 0x00, 0x08,
/* #1.68, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_03, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x60, 0x00, 0x00, 0x00, 0x08,
/* #1.69, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_04, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x64, 0x00, 0x00, 0x00, 0x08,
/* #1.70, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_05, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x68, 0x00, 0x00, 0x00, 0x08,
/* #1.71, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_06, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x6C, 0x00, 0x00, 0x00, 0x08,
/* #1.72, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_07, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x70, 0x00, 0x00, 0x00, 0x08,
/* #1.73, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_08, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x74, 0x00, 0x00, 0x00, 0x08,
/* #1.74, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_09, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x78, 0x00, 0x00, 0x00, 0x08,
/* #1.75, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_10, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x7C, 0x00, 0x00, 0x00, 0x08,
/* #1.76, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_11, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x80, 0x00, 0x00, 0x00, 0x08,
/* #1.77, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_12, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x84, 0x00, 0x00, 0x00, 0x08,
/* #1.78, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_13, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x88, 0x00, 0x00, 0x00, 0x08,
/* #1.79, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_14, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x8C, 0x00, 0x00, 0x00, 0x08,
/* #1.80, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_15, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x90, 0x00, 0x00, 0x00, 0x08,
/* #1.81, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_16, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x94, 0x00, 0x00, 0x00, 0x08,
/* #1.82, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_17, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x98, 0x00, 0x00, 0x00, 0x08,
/* #1.83, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_18, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0x9C, 0x00, 0x00, 0x00, 0x08,
/* #1.84, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_19, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xA0, 0x00, 0x00, 0x00, 0x08,
/* #1.85, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_20, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xA4, 0x00, 0x00, 0x00, 0x08,
/* #1.86, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_21, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xA8, 0x00, 0x00, 0x00, 0x08,
/* #1.87, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_22, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xAC, 0x00, 0x00, 0x00, 0x08,
/* #1.88, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_23, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xB0, 0x00, 0x00, 0x00, 0x08,
/* #1.89, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_24, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xB4, 0x00, 0x00, 0x00, 0x08,
/* #1.90, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_25, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xB8, 0x00, 0x00, 0x00, 0x08,
/* #1.91, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_26, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xBC, 0x00, 0x00, 0x00, 0x08,
/* #1.92, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_27, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xC0, 0x00, 0x00, 0x00, 0x08,
/* #1.93, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_28, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xC4, 0x00, 0x00, 0x00, 0x08,
/* #1.94, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_29, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xC8, 0x00, 0x00, 0x00, 0x08,
/* #1.95, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_30, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xCC, 0x00, 0x00, 0x00, 0x08,
/* #1.96, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_31, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xD0, 0x00, 0x00, 0x00, 0x08,
/* #1.97, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_32, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xD4, 0x00, 0x00, 0x00, 0x08,
/* #1.98, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_33, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xD8, 0x00, 0x00, 0x00, 0x08,
/* #1.99, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_34, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xDC, 0x00, 0x00, 0x00, 0x08,
/* #1.100, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_35, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xE0, 0x00, 0x00, 0x00, 0x08,
/* #1.101, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_36, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xE4, 0x00, 0x00, 0x00, 0x08,
/* #1.102, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_37, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xE8, 0x00, 0x00, 0x00, 0x08,
/* #1.103, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_38, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xEC, 0x00, 0x00, 0x00, 0x08,
/* #1.104, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_39, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xF0, 0x00, 0x00, 0x00, 0x08,
/* #1.105, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_40, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xF4, 0x00, 0x00, 0x00, 0x08,
/* #1.106, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_41, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xF8, 0x00, 0x00, 0x00, 0x08,
/* #1.107, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_00, value: 0x08, size: 4 */
0x40, 0x0E, 0x82, 0xFC, 0x00, 0x00, 0x00, 0x08,
/* #1.108, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_01, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x00, 0x00, 0x00, 0x00, 0x08,
/* #1.109, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_02, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x04, 0x00, 0x00, 0x00, 0x08,
/* #1.110, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_03, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x08, 0x00, 0x00, 0x00, 0x08,
/* #1.111, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_04, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x0C, 0x00, 0x00, 0x00, 0x08,
/* #1.112, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_05, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x10, 0x00, 0x00, 0x00, 0x08,
/* #1.113, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_06, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x14, 0x00, 0x00, 0x00, 0x08,
/* #1.114, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_07, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x18, 0x00, 0x00, 0x00, 0x08,
/* #1.115, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_08, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x1C, 0x00, 0x00, 0x00, 0x08,
/* #1.116, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_09, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x20, 0x00, 0x00, 0x00, 0x08,
/* #1.117, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_10, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x24, 0x00, 0x00, 0x00, 0x08,
/* #1.118, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_11, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x28, 0x00, 0x00, 0x00, 0x08,
/* #1.119, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_12, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x2C, 0x00, 0x00, 0x00, 0x08,
/* #1.120, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_13, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x30, 0x00, 0x00, 0x00, 0x08,
/* #1.121, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_14, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x34, 0x00, 0x00, 0x00, 0x08,
/* #1.122, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_15, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x38, 0x00, 0x00, 0x00, 0x08,
/* #1.123, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_16, value: 0x08, size: 4 */
0x40, 0x0E, 0x83, 0x3C, 0x00, 0x00, 0x00, 0x08,
/* #1.124, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_02, value: 0x08, size: 4 */
0x40, 0x0E, 0x84, 0x00, 0x00, 0x00, 0x00, 0x08,
/* #1.125, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_03, value: 0x08, size: 4 */
0x40, 0x0E, 0x84, 0x04, 0x00, 0x00, 0x00, 0x08,
/* #1.126, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_04, value: 0x08, size: 4 */
0x40, 0x0E, 0x84, 0x08, 0x00, 0x00, 0x00, 0x08,
/* #1.127, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_05, value: 0x08, size: 4 */
0x40, 0x0E, 0x84, 0x0C, 0x00, 0x00, 0x00, 0x08,
/* #1.128, command: write_value, address: SEMC_MCR, value: 0x10000004, size: 4 */
0x40, 0x0D, 0x40, 0x00, 0x10, 0x00, 0x00, 0x04,
/* #1.129, command: write_value, address: SEMC_BMCR0, value: 0x81, size: 4 */
0x40, 0x0D, 0x40, 0x08, 0x00, 0x00, 0x00, 0x81,
/* #1.130, command: write_value, address: SEMC_BMCR1, value: 0x81, size: 4 */
0x40, 0x0D, 0x40, 0x0C, 0x00, 0x00, 0x00, 0x81,
/* #1.131, command: write_value, address: SEMC_BR0, value: 0x8000001D, size: 4 */
0x40, 0x0D, 0x40, 0x10, 0x80, 0x00, 0x00, 0x1D,
/* #1.132, command: write_value, address: SEMC_SDRAMCR0, value: 0xF32, size: 4 */
0x40, 0x0D, 0x40, 0x40, 0x00, 0x00, 0x0F, 0x31,/*0x32,*/
/* #1.133, command: write_value, address: SEMC_SDRAMCR1, value: 0x772A22, size: 4 */
0x40, 0x0D, 0x40, 0x44, 0x00, 0x77, 0x2A, 0x22,
/* #1.134, command: write_value, address: SEMC_SDRAMCR2, value: 0x10A0D, size: 4 */
0x40, 0x0D, 0x40, 0x48, 0x00, 0x01, 0x0A, 0x0D,
/* #1.135, command: write_value, address: SEMC_SDRAMCR3, value: 0x21210408, size: 4 */
0x40, 0x0D, 0x40, 0x4C, 0x21, 0x21, 0x05/*0x04*/, 0x08,
/* #1.136, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
0x40, 0x0D, 0x40, 0x90, 0x80, 0x00, 0x00, 0x00,
/* #1.137, command: write_value, address: SEMC_IPCR1, value: 0x02, size: 4 */
0x40, 0x0D, 0x40, 0x94, 0x00, 0x00, 0x00, 0x02,
/* #1.138, command: write_value, address: SEMC_IPCR2, value: 0x00, size: 4 */
0x40, 0x0D, 0x40, 0x98, 0x00, 0x00, 0x00, 0x00,
/* #1.139, command: write_value, address: SEMC_IPCMD, value: 0xA55A000F, size: 4 */
0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0F,
/* #2, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #3, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #4, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #5, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #6, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #7.1-2, command header bytes for merged 'Write - value' command */
0xCC, 0x00, 0x14, 0x04,
/* #7.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */
0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,
/* #7.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
/* #8, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #9, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #10, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #11, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #12, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #13.1-2, command header bytes for merged 'Write - value' command */
0xCC, 0x00, 0x14, 0x04,
/* #13.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */
0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,
/* #13.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
/* #14, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #15, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #16, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #17, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #18, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #19.1-3, command header bytes for merged 'Write - value' command */
0xCC, 0x00, 0x1C, 0x04,
/* #19.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */
0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,
/* #19.2, command: write_value, address: SEMC_IPTXDAT, value: 0x33, size: 4 */
0x40, 0x0D, 0x40, 0xA0, 0x00, 0x00, 0x00, 0x33,
/* #19.3, command: write_value, address: SEMC_IPCMD, value: 0xA55A000A, size: 4 */
0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0A,
/* #20, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #21, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #22, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #23, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #24, command: nop */
0xC0, 0x00, 0x04, 0x00,
/* #25.1-2, command header bytes for merged 'Write - value' command */
0xCC, 0x00, 0x14, 0x04,
/* #25.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */
0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,
/* #25.2, command: write_value, address: SEMC_SDRAMCR3, value: 0x21210409, size: 4 */
0x40, 0x0D, 0x40, 0x4C, 0x21, 0x21, 0x05/*0x04*/, 0x09
};
/* BE CAREFUL MODIFYING THIS SETTINGS - IT IS YAML SETTINGS FOR TOOLS */

#else
const uint8_t dcd_data[] = {0x00};
#endif /* XIP_BOOT_HEADER_DCD_ENABLE */
#endif /* XIP_BOOT_HEADER_ENABLE */

And I also have another testing for clock_config.c

revolutesea_0-1648195668991.png

Just wanna SDRAM clock get any change..

revolutesea_1-1648195689032.png

Thank you,

 

标签 (1)
0 项奖励
回复
1 解答
968 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, assume you use the DCD to initialize the SDRAM, it's unnecessary to update the clock of SEMC actually.
Next, back to your below question,
1) Could you provide the example for 166MHz SDRAM or clearfy why I am unable to reduce the SDRAM clock?
-- I'd like to suggest you to modify the semc which resides in the ~\boards\evkmimxrt1170\driver_examples\semc to implement access the SDRAM on your board, after that, you can adjust the DCD by referring to the detailed values of the SEMC's registers.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
958 次查看
revolutesea
Contributor II

Thank you!

0 项奖励
回复
969 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, assume you use the DCD to initialize the SDRAM, it's unnecessary to update the clock of SEMC actually.
Next, back to your below question,
1) Could you provide the example for 166MHz SDRAM or clearfy why I am unable to reduce the SDRAM clock?
-- I'd like to suggest you to modify the semc which resides in the ~\boards\evkmimxrt1170\driver_examples\semc to implement access the SDRAM on your board, after that, you can adjust the DCD by referring to the detailed values of the SEMC's registers.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------