Series Termination for LVDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Series Termination for LVDS

974 Views
vigneshvasudeva
Contributor II

Is it necessary to provide series termination resistor at LVDS data and clock lines of I.MX6?

If yes, what value is preferred?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

638 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vignesh

IMX6DQ6SDLHDG sect.3.10 LVDS recommendations

Use the following recommendations for the LVDS.

• Follow standard high-speed differential routing rules for signal integrity.

• Each differential pair should be length matched to ± 5 mils.

• LVDS differential pairs should have a differential impedance of 100 Ω.

If it is standard LVDS LCD it already has proper input termination.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply