Serial download detail process

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Serial download detail process

跳至解决方案
446 次查看
BryceWang
Contributor II

I read i.MX RT1050 RM.

- In chapter 9.9, Is fig 9-18 the handshake process between host and chip?Or does it only happen on the chip side?

- About serial download protocol (SDP), when host communication with chip, is need response to each other when accept report. For example, SDP commands is WRITE_FILE. In my understanding, host send report1 to chip first, and then host send data to chip. If the first step fail, such as chip not receive the report1, what happend? When chip receives report1, will it send a response to the host?

Thank you!

标记 (1)
0 项奖励
回复
1 解答
359 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @BryceWang 

Yes, SDPHOST is meant to be used from host to chip. 

We do not provide the source code, but the executable. 

You can find  the SDPHOST and other related tools in this package Flash loader i.MX RT1060/1040 package

Best regards, 

Diego

 

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
382 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @BryceWang 

I hope that you are doing great! 

To my understanding fig 9-18  is the boot flow when the MCU is set to boot in serial downloader. The ROM will wait for any commands from the Host, over LPUART1 or USB1 interfaces. This command could be as simple as the following example.

sdphost -u 0x1FC9,0x0130 -j -- error-status

To which the boot ROM will simply reply as shown in the below  figure. The error command works as a simple ping command,  that the host sends to discover if the MCU is active. 

diego_charles_0-1706141183722.png

Below I provide an example, where the command write-file is used. Each command issued from the host receives a response. 

diego_charles_1-1706141732646.png

If the MCU is not in serial downloader mode, there won't be any responses from the host. 

I hope this could help, 

Diego

 

0 项奖励
回复
370 次查看
BryceWang
Contributor II

Hi @diego_charles 

In your answer, you use sdphost to communication from host to chip. How can i get sdphost source code?

Thanks for your answer

0 项奖励
回复
360 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @BryceWang 

Yes, SDPHOST is meant to be used from host to chip. 

We do not provide the source code, but the executable. 

You can find  the SDPHOST and other related tools in this package Flash loader i.MX RT1060/1040 package

Best regards, 

Diego

 

 

0 项奖励
回复
431 次查看
BryceWang
Contributor II

BryceWang_0-1705641468868.png

 

0 项奖励
回复