Hello,
I'm trying to run a simple OpenGL application with the DirectFB enabled vivante libraries from gpu-viv-bin-mx6q. When trying to initialize EGL I get a segmentation fault in what i guess is the libEGL-dfb.so. The callstack is as follows:
GetDFBSurfFormat() at gc_hal_user_dfb.c:61 0x2af52a50
gcoOS_GetWindowInfoEx() at gc_hal_user_dfb.c:1,191 0x2af53524
veglGetWindowInfo() at gc_egl_platform.c:139 0x2ac57ce8
_CreateSurface() at gc_egl_surface.c:1,690 0x2ac52bd4
eglCreateWindowSurface() at gc_egl_surface.c:2,712 0x2ac5381c
init() at SimpleTriangle.c:213 0x9a7c
main() at SimpleTriangle.c:353 0xa224
I'm trying to initialize the EGL with the following code:
DFBResult err;
DFBSurfaceDescription dsc;
DFBCHECK(DirectFBInit(&argc, &argv));
// create the super interface
DFBCHECK(DirectFBCreate(&dfb));
// create an event buffer for all devices with these caps
DFBCHECK(dfb->CreateInputEventBuffer(dfb, DICAPS_KEYS | DICAPS_AXES, DFB_FALSE, &events));
// set our cooperative level to DFSCL_FULLSCREEN for exclusive access to the primary layer
dfb->SetCooperativeLevel(dfb, DFSCL_FULLSCREEN);
// get the primary surface, i.e. the surface of the primary layer we have exclusive access to
dsc.flags = DSDESC_CAPS;
dsc.caps = DSCAPS_PRIMARY | DSCAPS_DOUBLE; // | DSCAPS_OPENGL_HINT;
DFBCHECK(dfb->CreateSurface(dfb, &dsc, &primary));
// get the size of the surface and fill it
//DFBCHECK(primary->GetSize(primary, &screen_width, &screen_height));
//DFBCHECK(primary->FillRectangle(primary, 0, 0, screen_width, screen_height));
egldisplay = eglGetDisplay(EGL_DEFAULT_DISPLAY);
eglInitialize(egldisplay, NULL, NULL);
assert(eglGetError() == EGL_SUCCESS);
eglBindAPI(EGL_OPENGL_ES_API);
eglChooseConfig(egldisplay, s_configAttribs, &eglconfig, 1, &numconfigs);
assert(eglGetError() == EGL_SUCCESS);
assert(numconfigs == 1);
eglsurface = eglCreateWindowSurface(egldisplay, eglconfig, (EGLNativeWindowType)primary, NULL);
Has anybody experienced something similar or do you have a working example with this configuration?
Regards,
David
ChucoChe Apr 14, 2014 11:54 AM (in response to imxcommunityscout)
Hi,
Is there an error displayed by DirectFB when you get the segmentation fault?
DirectFB gets it's memory from FBdev pool, to increase the memory for FBdev use fbset.
For example:
fbset -fb /dev/fb0 -g 1024 768 1024 2304 24
That may solve your issue.
Also find below our EGL code to get native display and window in the yocto BSP:
#include <directfb.h>
struct _DFBDisplay
{
IDirectFB* pDirectFB;
IDirectFBDisplayLayer* pLayer;
IDirectFBEventBuffer* pEventBuffer;
int winWidth, winHeight;
};
struct _DFBWindow
{
IDirectFBWindow* pWindow;
IDirectFBSurface* pDFBSurf;
};
struct _DFBDisplay* display = NULL;
struct _DFBWindow *DFBWindow = NULL;
IDirectFBWindow *window = NULL;
EGLNativeDisplayType fsl_getNativeDisplay()
{
EGLNativeDisplayType eglNativeDisplayType = NULL;
printf("getting display \n");
DFBDisplayLayerConfig config;
if(DirectFBInit(NULL, NULL) != DFB_OK)
{
printf("DFBinit failed \n");
return 0;
}
display = (struct _DFBDisplay*) malloc(sizeof (struct _DFBDisplay));
if (display == NULL)
{
printf("allocation failed \n");
return 0;
}
if (DirectFBCreate(&(display->pDirectFB)) != DFB_OK)
{
printf("DirectFBCreate failed \n");
return 0;
}
if(display->pDirectFB->CreateInputEventBuffer(display->pDirectFB, DICAPS_KEYS, DFB_FALSE, &(display->pEventBuffer)) != DFB_OK)
{
printf("CreateInputEventBuffer failed \n");
return 0;
}
if(display->pDirectFB->GetDisplayLayer( display->pDirectFB, DLID_PRIMARY, &(display->pLayer) ) != DFB_OK)
{
printf("GetDisplayLayer failed \n");
return 0;
}
display->pLayer->GetConfiguration(display->pLayer, &config);
display->winWidth = config.width;
display->winHeight = config.height;
printf("getting display succed\n");
eglNativeDisplayType = (EGLNativeDisplayType)display;
return eglNativeDisplayType;
}
EGLNativeWindowType fsl_createwindow(EGLDisplay egldisplay, EGLNativeDisplayType eglNativeDisplayType)
{
EGLNativeWindowType native_window = (EGLNativeWindowType)0;
printf("getting window \n");
DFBWindowDescription desc;
display->pLayer->SetCooperativeLevel( display->pLayer, DLSCL_ADMINISTRATIVE );
DFBWindow = (struct _DFBWindow *) malloc(sizeof(struct _DFBWindow));
memset(DFBWindow, 0, sizeof(struct _DFBWindow));
desc.flags = ( DWDESC_POSX | DWDESC_POSY);
desc.posx = 0;
desc.posy = 0;
display->winWidth = 640;
display->winHeight = 480;
desc.flags = desc.flags | DWDESC_WIDTH | DWDESC_HEIGHT;
desc.width = 640;
desc.height = 480;
desc.surface_caps = DSCAPS_FLIPPING;
if(display->pLayer->CreateWindow( display->pLayer, &desc, &window) != DFB_OK)
{
printf("CreateWindow failed \n");
return 0;
}
DFBWindow->pWindow = window;
window->SetOpacity(window, 0xFF);
window->RaiseToTop(window);
window->AttachEventBuffer(window, display->pEventBuffer);
display->pLayer->EnableCursor(display->pLayer, 0);
native_window = (EGLNativeWindowType) DFBWindow;
assert(native_window);
printf("getting window succed \n");
return native_window:
}
Michel
Vivante team has acknowledged and fixed these bugs . however it looks like you are using a vivante driver old version The fixes were included in the Vivante 4.6.9p11 driver, the latest bsp in FSL web includes the 4.6.13p
Also, This issue happen on Sabre board or your custom board?
Could you check your board file for the GPU reserved memory?
For example on sabreSD, the following code is used to reserve gpu memory which is limited under 1G address.
Arch/arm/mach-mx6/board-mx6q_sabresd.c
if (imx6q_gpu_pdata.reserved_mem_size) {
phys = memblock_alloc_base(imx6q_gpu_pdata.reserved_mem_size,
SZ_4K, SZ_1G);
memblock_remove(phys, imx6q_gpu_pdata.reserved_mem_size);
imx6q_gpu_pdata.reserved_mem_base = phys;
}
Hope this helps
regards