Saving Vcc power with i.MX537

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Saving Vcc power with i.MX537

ソリューションへジャンプ
956件の閲覧回数
TedMichon
Contributor I

I understand the DVFS concept with Vdd, but how does it work with Vcc? With Vdd, we just slow the CPU clock, and therefore can lower the voltage and save power while we aat idle or in background.

But with Vcc, we cannot lower the FEC or USB or UART clocks without causing the these systems to fail because they need specific clock rates. How does one save power with DVFS for Vcc?

-Ted

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
819件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Ted

     The DVFS includes CORE and PER, the CORE means CPU, and PER means peripheral, once there is no high speed devices running, dvfs per driver can lower bus's freq, includes DDR, AXI, AHB etc., and with lower bus freq, Vcc can be lower as well.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
819件の閲覧回数
YixingKong
Senior Contributor IV

Ted

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信
819件の閲覧回数
YixingKong
Senior Contributor IV

Ted

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信
820件の閲覧回数
AnsonHuang
NXP Employee
NXP Employee

Hi, Ted

     The DVFS includes CORE and PER, the CORE means CPU, and PER means peripheral, once there is no high speed devices running, dvfs per driver can lower bus's freq, includes DDR, AXI, AHB etc., and with lower bus freq, Vcc can be lower as well.

0 件の賞賛
返信