SabreSD board unable to capture & display 1080P30

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SabreSD board unable to capture & display 1080P30

Jump to solution
1,546 Views
ottob
Contributor IV

Hi There,

We need to be able to capture (parallel CSI) and display HD video on our product based on the iMX6. However, we run into a problem with high-CPU usage and dropped frames. The problem is easily reproduced on the SabreSD development board.

This 720P pipeline shows 14% usage in top, meaning it uses more than 50% of one processor if I'm not mistaken. There appears to be no frames dropped

gst-launch mfw_v4lsrc capture-mode=4 device=/dev/video1 ! mfw_v4lsink

Running time 0:01:00.329872674 render fps 29.985


However, when switching to 1080P the situation gets significantly worse. Top shows 25%, meaning one CPU is used %100. About 15% of the frames are dropped.

gst-launch mfw_v4lsrc capture-mode=5 device=/dev/video1 ! mfw_v4lsink

Running time 0:01:04.074657008 render fps 24.487

Not being able to capture and display full HD material in 30FPS is a very serious problem for us, so we are hoping this can be resolved soon.

Btw, the SabreSD camera is using MIPI CSI capture while we are using the parallel CSI on our board, but the performance appears to be about the same.

Any help or hints would be appreciated

Thanks

/Otto

Using iMX6Q on Yocto GA1.0.0

Labels (4)
0 Kudos
1 Solution
1,131 Views
Yuri
NXP Employee
NXP Employee

1.
Please try to use "mfw_v4isink" instead of "mfw_v4lsink".

2.
As for the VPU - as I see - the VPU is not involved in Your pipeline.
Just as a demo example :


$ gst-launch mfw_v4lsrc device=/dev/video1 ! vpuenc  codec=6 ! matroskamux ! queue max-size-bytes=0 max-size-time=0 ! vpudec ! mfw_v4lsink

Please pay attention, both operations (encoding and decoding - just for demo) are used here !

Usually encoding is applied on one board, while the decoding - on the other one, connected via Etherenet.

Regards,

Yuri.

View solution in original post

0 Kudos
6 Replies
1,131 Views
ottob
Contributor IV

Update - I tried increasing the VPU frequency to 352Mhz, which reduced the CPU usage on our platform from 21% to 18% when capturing 1080i. I do not have a build-platform set up for building a clean SabreSD kernel with the 352MHz VPU option enabled, but I think its safe to assume the CPU usage will drop a few percent there as well maybe enough for it to be able to capture 1080P30 without any dropped frames. Still does not explain why capturing video and displaying it uses up essentially 100% of one core. Shouldn't DMA be used ? Can it be used ?

Thanks,

/Otto

Btw, I'll set up a clean build environment for the SabreSD board so I can go more general testing

0 Kudos
1,131 Views
ottob
Contributor IV

Minor update - Increasing the VPU frequency on SabreSD board did not lead to any significant improvement. "Top" still showing 25% usage (100% of one Core)

root@imx6qsabresd:/# cat /sys/kernel/debug/clk/clk_summary | grep vpu

          vpu_axi_sel           0           0            352000000

             vpu_axi_podf       0           0            352000000

                vpu_axi         0           0            352000000

gst-launch mfw_v4lsrc capture-mode=5 device=/dev/video1 ! mfw_v4lsink

Running time 0:02:03.897685014 render fps 24.504

Setting pipeline to READY ...

Setting pipeline to NULL ...

Total rendered:3036

Freeing pipeline ...

[--->FINALIZE v4l_sink

0 Kudos
1,132 Views
Yuri
NXP Employee
NXP Employee

1.
Please try to use "mfw_v4isink" instead of "mfw_v4lsink".

2.
As for the VPU - as I see - the VPU is not involved in Your pipeline.
Just as a demo example :


$ gst-launch mfw_v4lsrc device=/dev/video1 ! vpuenc  codec=6 ! matroskamux ! queue max-size-bytes=0 max-size-time=0 ! vpudec ! mfw_v4lsink

Please pay attention, both operations (encoding and decoding - just for demo) are used here !

Usually encoding is applied on one board, while the decoding - on the other one, connected via Etherenet.

Regards,

Yuri.

0 Kudos
1,131 Views
ottob
Contributor IV

Thanks a lot for your help Yuri ! CPU usage is now shown as 0% in top

0 Kudos
1,131 Views
Yuri
NXP Employee
NXP Employee

I hope some hints below helps.

1. Please use "mfw_v4lsrc" element.

"VPU performance: CSI-2 MIPI camera vs. USB camera"

https://community.freescale.com/message/394777#394777

2. It is not clear if VPU is used in the Gstreamer pipeline.

VPU using can decrease system load because of coding raw camera data.

Regards,

Yuri.

0 Kudos
1,131 Views
ottob
Contributor IV

Yuri,

I generalized the post after making some discoveries. Preferably I would have liked to delete the post and add a new one but it did not allow me.

Any thoughts on how to solve this ?

Thanks !

/Otto

0 Kudos