Sabre-DDR3 M7 and T7 balls connect to IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sabre-DDR3 M7 and T7 balls connect to IMX6

ソリューションへジャンプ
844件の閲覧回数
joseantoniomoya
Contributor I

Hello.

I´m checking the squematic of Sabre board and the datasheet MT41K128M16JT and i see the M7,T7 balls conect to IMX6, but the MT41K128M16JT datasheet this balls are "NC".

Why are they connected?


Best Regards

ラベル(1)
タグ(4)
0 件の賞賛
1 解決策
638件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jose

this is done for compatibility with design with larger memories

(pinout is standard). In general one can solder memory chip with larger memory size.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
639件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jose

this is done for compatibility with design with larger memories

(pinout is standard). In general one can solder memory chip with larger memory size.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
638件の閲覧回数
joseantoniomoya
Contributor I
I understand.  Thank you.
0 件の賞賛