Sabre-DDR3 M7 and T7 balls connect to IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sabre-DDR3 M7 and T7 balls connect to IMX6

Jump to solution
801 Views
joseantoniomoya
Contributor I

Hello.

I´m checking the squematic of Sabre board and the datasheet MT41K128M16JT and i see the M7,T7 balls conect to IMX6, but the MT41K128M16JT datasheet this balls are "NC".

Why are they connected?


Best Regards

Labels (1)
Tags (4)
0 Kudos
1 Solution
595 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jose

this is done for compatibility with design with larger memories

(pinout is standard). In general one can solder memory chip with larger memory size.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
596 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jose

this is done for compatibility with design with larger memories

(pinout is standard). In general one can solder memory chip with larger memory size.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
595 Views
joseantoniomoya
Contributor I
I understand.  Thank you.
0 Kudos