Sabre-DDR3 M7 and T7 balls connect to IMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sabre-DDR3 M7 and T7 balls connect to IMX6

跳至解决方案
803 次查看
joseantoniomoya
Contributor I

Hello.

I´m checking the squematic of Sabre board and the datasheet MT41K128M16JT and i see the M7,T7 balls conect to IMX6, but the MT41K128M16JT datasheet this balls are "NC".

Why are they connected?


Best Regards

标签 (1)
标记 (4)
0 项奖励
1 解答
597 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jose

this is done for compatibility with design with larger memories

(pinout is standard). In general one can solder memory chip with larger memory size.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
2 回复数
598 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jose

this is done for compatibility with design with larger memories

(pinout is standard). In general one can solder memory chip with larger memory size.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
597 次查看
joseantoniomoya
Contributor I
I understand.  Thank you.
0 项奖励