SPL spends 1.5 seconds

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPL spends 1.5 seconds

跳至解决方案
1,481 次查看
hjpark71
Contributor III

Hi Guys,

I found very strange number from booting speed measurement on variscite board what uses I.MAX6Q.

Please found the RED on the log from SPL. As see, it spends 1.5 seconds.

Do you know why this SPL is so slow on eMMC ?

Is it a bug on the code or H/W problem?

FYI, this u-boot is from "git clone https://github.com/varigit/uboot-imx"

[0.000001 0.000001]

[0.001007 0.001006] U-Boot SPL 2015.04-14426-gf45bfc9 (Jul 05 2016 - 15:24:26)
[0.062982 0.061975]
[0.063943 0.000961] Part number: VSM-DT6-302
[0.066099 0.002156] Assembly: AS160306088
[0.068105 0.002006] Date of production: 2016 Apr 13
[1.553261 1.485156] MMC Boot Device: mmc1 (eMMC)
[1.697154 0.143893]
[1.697221 0.000067] U-Boot 2015.04-14426-gf45bfc9 (Jul 05 2016 - 15:24:26)
[1.702165 0.004944]
[1.702240 0.000075] CPU: Freescale i.MX6Q rev1.5 at 792 MHz
[1.716127 0.013887] CPU: Temperature 47 C
[1.718401 0.002274] Reset cause: POR
[1.719626 0.001225] Board: Variscite VAR-SOM-MX6 Quad-PoP 792 MHz
[1.723541 0.003915] I2C: ready
[1.725097 0.001556] DRAM: 1 GiB
[1.768103 0.043006] PMIC: PFUZE100 ID=0x10
[1.781095 0.012992] MMC: FSL_SDHC: 0, FSL_SDHC: 1
[1.910019 0.128924] auto-detected panel VAR-WVGA
[1.913123 0.003104] Display: VAR-WVGA (800x480)
[2.124984 0.211861] In: serial
[2.127038 0.002054] Out: serial
[2.128119 0.001081] Err: serial
[2.249945 0.121826] switch to partitions #0, OK
[2.253238 0.003293] mmc1(part 0) is current device
[2.255963 0.002725] eMMC: 7.3 GiB
[2.257182 0.001219] Net: using phy at 7
[2.285979 0.028797] FEC [PRIME]
[2.287958 0.001979] Normal Boot
[2.288947 0.000989] Hit any key to stop autoboot: 1     0
[3.413281 1.124334] switch to partitions #0, OK
[3.416414 0.003133] mmc1(part 0) is current device
[3.544225 0.127811] ** No boot file defined **
[3.551236 0.007011] reading uImage
[3.837130 0.285894] 5958784 bytes read in 286 ms (19.9 MiB/s)
[3.841167 0.004037] Booting from mmc ...
[3.847103 0.005936] reading imx6q-var-dart.dtb
[3.866032 0.018929] 43160 bytes read in 18 ms (2.3 MiB/s)
[3.869161 0.003129] ## Booting kernel from Legacy Image at 12000000 ...
[3.874070 0.004909] Image Name: Linux-4.1.15-gb8788ad
[3.877279 0.003209] Image Type: ARM Linux Kernel Image (uncompressed)
[3.882204 0.004925] Data Size: 5958720 Bytes = 5.7 MiB
[3.886116 0.003912] Load Address: 10008000
[3.888205 0.002089] Entry Point: 10008000
[3.891060 0.002855] Verifying Checksum ... OK
[3.961982 0.070922] ## Flattened Device Tree blob at 18000000
[3.965113 0.003131] Booting using the fdt blob at 0x18000000
[3.969140 0.004027] Loading Kernel Image ... OK
[4.044020 0.074880] Using Device Tree in place at 18000000, end 1800d897
[4.051925 0.007905] switch to ldo_bypass mode!
[4.054825 0.002900]
[4.054935 0.000110] Starting kernel ...

标签 (1)
0 项奖励
1 解答
1,097 次查看
JohnDoe1z
Contributor III
0 项奖励
3 回复数
1,098 次查看
JohnDoe1z
Contributor III

Try to apply this patch and see if it helps:

[U-Boot] [PATCH] arm: mx6: Reduce SPL malloc pool size

0 项奖励
1,097 次查看
hjpark71
Contributor III

Hi John

Before I met your answer, I added more debugging code into SPL and found a code which takes 1.5 secs in SPL. it is

#ifdef CONFIG_SYS_MALLOC_CLEAR_ON_INIT

memset((void *)mem_malloc_start, 0x0, size);

debug("mem_malloc_init(1)\n");

#endif

I didn't know the size is 50MB but you gave me the right answer.. thanks a lot..

0 项奖励
1,097 次查看
igorpadykov
NXP Employee
NXP Employee

Hi hj

spl is not supported in nxp bsp releases, however one can try fast boot:

imx6q, eMMC fast boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励